Smart Limit Watcher provides real time machine monitoring and alerting to improve your plant preventive maintenance initiatives.
moneo’s Smart Limit Watcher uses 3 proven and widely accepted statistical algorithm models constructed specifically for industrial automation.
But you don't need to be an expert on these algorithm models! Using its graphical interface designed specifically for industrial automation, the Smart Limit Watcher guides you through the entire process of assigning the necessary measurements to automatically implement the correct model to your application. The guided tour video below demonstrates this simplicity.
Smart Limit Watcher automatically sets up confidence bands based on data from "good condition" training.
There are two main application methods for which the Smart Limit Watcher can be applied to most industrial machines.
Supportive (Vertical) measurements
Comparative (Horizontal) measurements
Compression system condition monitoring
Method: Supportive (Vertical) measurements
The Smart Limit Watcher tracks the mechanical health using the vibration signal V-RMS for potential wear. This measurement has the strongest influence on the compressor availability, so it is identified as the target variable.
Support variables include current amps and rotational speed of the motor, system pressure and system temperature.
Item | Sensor | Variable | Measurement description |
---|---|---|---|
1 | VVB vibration sensors |
Target | Vibration is the primary measurement for mechanical condition.
|
2 | Motor current sensors |
Support | Motor current indicates total energy used to power the work produced by the compressor.
|
3 | DI compact speed sensors |
Support | Rotational speed is a significant indicator of motion and directly impacts changes in vibration.
|
4 | TS RTDs and TR tempeature sensors |
Support | Temperature is linked as another form of energy loss.
|
5 | PN pressure sensors |
Support | Pressure is the work output of the compressor.
|
Multiple conveyor drive motor condition monitoring
Method: Comparative (Horizontal) measurements
Applying the Smart Limit Watcher to a conveyor with multiple drive systems compares how each drive operates in relation to the others. The vibration measurement V-RMS compares the mechanical integrity of the rotating components and the quality of their connection to the complete conveyor system. Any drive system that performs differently than the others is identified.
In this implementation each of the variables have an equal weight to their relevance.
Sensor | Variable | Measurement description |
---|---|---|
VVB vibration sensors |
Target and suport | Vibration is used as the primary measurement for mechanical condition.
|