Safety at Work (SAW) has been available since 2000 as the first approved safety networking technology. SAW is an approved safety network that incorporates the required international safety approvals for functional safety. The system is certified by TUV, a Nationally Recognized Testing Laboratory that is recognized by OSHA.
Each fail-safe AS-i slave has a unique code sequence that is 8 x 4 bits. While the contacts are in the closed position, a 32 bit number is transmitted over the AS-i cable 4 bits at a time. After eight scans, the pattern repeats. The bit pattern is referred to as a "Code Table".
The fail-safe AS-i slave responds to each cyclic data call of the AS-i master with one of the following:
The AS-i safety monitor only listens to the communication between the AS-i master and fail-save AS-i slave. The safety monitor also knows the code sequence of each configured safe AS-i slave because it is taught during set-up. The safety monitor safely switches off its output if the c ode sequence is received incompletely or not at all.
IP rating | Certifications | Features | |
---|---|---|---|
AS-i safety monitor | IP 20 | SIL 3 SILcl 3 PL e Cat. 4 |
|
Part numbers | Description | IP rating | Certifications | Inputs | Outputs |
---|---|---|---|---|---|
AC009S / AC030S | Control cabinet module | IP 20 | SIL 3 SILcl 3 PL e Cat. 4 |
|
|
AC50xS | ClassicLine with quick mounting technology | IP 67 | SIL3 SILcl 3, SILcl 2 PL e Cat. 4, PL d Cat. 3 |
|
|
AC01xS | E-stop | IP 67 | SIL 3 SILcl 3 PL e Cat. 4 |
|
|
PCB solutions | With the help of AS-i PCBs mechanical switches can be integrated into AS-i networks | Depends on housing | SIL 3 PL e Cat. 4 |
|
|
AC90xS | Safety switch with guard locking | IP 67 | PL d |
|
|
Read more: What is AS-i protocol?