- O5D laser distance sensors
- Setup and support
- Device configuration
O5D laser distance sensors: Device configuration
The following will guide you through key programming steps for the O5D sensors. We highlight the features used most often here. Refer to the Operating Instructions manual found under the “Downloads” tab at the product datasheet page for more details on programming the sensors and other features.
The IO-Link enabled sensors can also be configured using the moneo | confgure software.
The O5D sensor displays distance to target in the units of measure set in the configuration menu.
Display and indications
| Element | Description | |
|---|---|---|
| 1 | Green LED | Lighting LED = Operation |
| 2 | YellowLED | Indication of switching status |
| 3 | 3-digit alphanumeric display | Indication of the measured value |
| 4 | Programming button | Range + |
| 5 | Programming button | Range - |
Setting the switch point
The sensor will switch when the object is detected.