• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain
  • my ifm
  1. TN temperature sensors
  2. Setup and support
  3. Installation guidelines

Installation guidelines - TN temperature sensors

The TN sensors are easy to apply. For best performance, please adhere to the following guidelines.

  • The RTD measuring element is in the tip of the probe. Insertion depth into the medium must be at least 12 mm.
  • The body of the sensor rotates so the display lines up as desired. Mount firmly into the process prior to adjusting the display.