• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • my ifm
  1. TN temperature sensors
  2. Setup and support

Installation guidelines - TN temperature sensors

The TN sensors are easy to apply. For best performance, please adhere to the following guidelines.

  • The RTD measuring element is in the tip of the probe. Insertion depth into the medium must be at least 12 mm.
  • The body of the sensor rotates so the display lines up as desired. Mount firmly into the process prior to adjusting the display.

Should you need additional support, feel free to contact our service center at 800-441-8246 and speak to one of our applications engineers.