• 製品
  • 産業別
  • IIoTソリューション
  • サービス
  • 会社案内

moneo release notes

moneo – simply made for you also means permanent optimisation of the software - regarding the platform as well as the modules. At regular intervals, we release free updates that come up with features and enhancements in several areas of the software, keeping your individual software packages up to date.

Here you can read all about the changes in the latest version and also access past release information.

The free update to the new moneo software version is now available in the downloads.

What's new in moneo? Click on the function tiles to see the new features of the software release.

Depending on the software licences you purchased, the visibility of the tiles in the moneo software may differ.

Monitoring table

List overview of process data

Previous innovations

Here you can find the complete release notes: moneo RTM

Dashboard

Graphical overview of process data

Previous innovations

Here you can find the complete release notes: moneo RTM

Analysis

Visualise historic data and data recordings

Here you can find the complete release notes: moneo RTM

Tasks and tickets

Overview of jobs to be done

Previous innovations

Here you can find the complete release notes: moneo RTM

Settings and rules

Define warning and alarm conditions

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo RTM

Device management

Onboard devices & set up topology structure

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo OS

Calculated values

Calculate additional information from existing datasources

Previous innovations

Here you can find the complete release notes: moneo OS

Connected devices

Configuration of connected devices

Previous innovations

Here you can find the complete release notes: moneo configure (SA)

Saved configurations

Management of saved device configurations

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo configure (SA)

Device descriptions

Management of IODDs and device descriptions...

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo configure (SA)

Data Science Toolbox

Predictive analytics

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo DataScience Toolbox

AVA raw data

Recording of vibration raw data

  • currently there is no new release information

Previous innovations

Here you can find the complete release notes: moneo RTM

AVA wizard

Vibration monitoring according to ISO 10816-3

  • currently there is no new release information

Here you can find the complete release notes: moneo RTM

edgeConnect

Set up target systems & map datasources

Previous innovations

Here you can find the complete release notes: moneo OS

Miscellaneous

General changes

Previous innovations

Appliance Management System

The ideal hardware with pre-installed software.

Here you can find the complete release notes: moneo appliance