When choosing the correct thermowell for a temperature sensor installation, there are two possible approaches:
The first and ideal approach is to choose the thermowell before the temperature sensor. This is because the thermowell’s process connection and installation length will be what is installed into your machine or application.
Below, we will explain the terms used on the datasheets of ifm thermowells and provide guidance on how to determine whether a thermowell and temperature device are compatible.
On the Industrial thermowells page and Sanitary thermowells page, you can find a variety of thermowells that ifm offers.
Using the above explanation of the thermowell datasheet, follow these steps:
These are the only two specifications that are important when choosing a thermowell. Once the proper thermowell is chosen based on the desired process connection and installation length, determine which temperature sensor is compatible with your chosen thermowell by using Approach 2.
Using the above explanation of the ifm temperature datasheet, the following four specifications are important when determining compatibility between a thermowell and temperature device:
Note: Compression fittings are offered as accessories for RTDs and temperature sensors with 6, 8 or 10 mm diameter probes. When a compression fitting is used, the probe's [1] EL specification needs to be at least 25 mm longer than [3] Design for temperature sensors EL in order to bottom out in the thermowell.
If an ifm temperature device is not being used:
The temperature devices's installation length or probe length will need to be determined and can subsitute [1] EL in step 1. The temperature device's [2] Process connection will also need to be confirmed for step 2.