• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. MVQ positioner solution
  2. Setup and support
  3. Device configuration

MVQ valve positioner: Device configuration

The following information will help you quickly program the IO-Link enabled valve positioner after installing your MVQ valve sensor. For more details, please refer to the operating instructions with the product datasheet.

Configuration with moneo

moneo | configure is a user-friendly software package that enables easy programming and visualization of all ifm IO-Link enabled sensors (V1.0 and V1.1) as well as other manufacturers' IO-Link enabled sensors (V1.1).  The software can be downloaded here: moneo | configure.

Smart phone running the moneo blue app and the EIO330 bluetooth adapter

moneo | blue is an app that runs on your Apple or Android smart phones and provides access to all parameters, process values and diagnostics from all sensors connected to an IO-Link master. The Bluetooth™ adapter, EIO330, connects to one port of the IO-Link master and the app can be downloaded free of charge from the Apple App Store or from Google play.

Electrical connection to the solenoid and IO-Link master

Configurating the MVQ positioner

Step-by-step configuration

The MVQ positioner can be configured very quickly with just 3 steps via moneo configure.

Step 1: Enable B-ports

B-type ports on an IO-Link master e.g., AL1422 are disabled by default. First connect the IO-Link master to moneo and enable the B-ports.

Step 2: Select valve rotation

Default setting: Counter clock-wise.

If your valve is counter clock-wise, you do not need to change this configuration.

Valve rotation parameter setting in moneo configure. Counter clock wise and clock wise are the options.

Step 3: Automatic valve setup

Under the “Valve setup” section, you will find “Advanced teach configuration”. Click on the dropdown button and you will find 2 options: Automatic valve setup and positioning tuning; and Automatic valve setup.

For quick setup, click on “Automatic valve setup” and write to the device, then click on “Execute command”.

The sensor will learn the current position of the valve, and study which solenoid should be energized and move the valve from 0% (close) to 100% (open). The teach is now done.

The User can then define the desired position and input it to the sensor.

Valve setup in moneo configure showing the advanced teach configuration parameter.

Visual feedback

The MVQ positioner provides clear feedback via its indicators and the control system when the desired position is reached. This allows operators to easily monitor and optimise processes, resulting in increased efficiency and productivity.

LED ring

The LED ring of the MVQ positioner offers a wide range of color options, including red, green, yellow, blue, magenta, cyan and white. The LEDs can be continuously lit or flashed at different frequencies to visualize different operating states. The colors can be individually selected and adapted via IO-Link to meet your application requirements.

 

Action Indication Color Default color
Advanced teach Flashes with a frequency of 1 Hz as long as the advanced teach is running. selectable via IO-Link: [OFF], [green], [blue], [yellow], [magenta], [cyan], [white] Default: [white] white
Within the deadband Lights when the actual value is in the deadband and control is completed. white
Control active Flashes with a frequency of 1 Hz as long as the control is active. OFF
Close Lights when the actual value is <= SC1.2. blue
Open Lights when the actual value is >= SC1.1. yellow
Locator Double flashing green
Error Flashes with a frequency of 1 Hz as long as the error is present. Minimum display time 3 seconds. red

Status LEDs

LED name Color Operating status
Green Statically on when the device is ready for operation.

Open
White Statically on when the valve is open.
(SC1.1 active)

Close
Statically on when the valve is closed.
(SC1.2 active)

In position
Statically on when the actual valve is in the deadband and control is completed.

Puck

Positionsanzeiger in MVQ Ventilsensor

The mechanical position indicator (puck) shows the valve position even when the device is not powered.