Thank you for your purchase of an SD compressed air flow meter to improve equipment performance. On the following pages, you will find information to help you install and program the sensor as well as answers to frequently asked questions about our air flow meter line.
Should you need additional support, feel free to contact our service center at 800-441-8246 and speak to one of our applications engineers.
Properly setting up an air flow meter offers several benefits, including:
Proper setup helps ensure that you will get precise air flow measurements.
Accurate, real-time data assists you with detecting leaks and other problems that cause your facility to use more compressed air or natural gas than necessary.
Reducing downtime and maintenence resources, along with utilizing fewer resources, cut costs and reduce expenses for a facility.
Compressed air leaks, and esepcially nautral gas leaks, are dangerous for workers in your facility. A properly-installed flow alerts you to even the smallest leaks. This process enables you to address these concerns before they gget worse or cause an injury.
Proper air flow meter setup is crucial for achieving accurate measurements. Read our overivew below or get more details on air flow meter setup:
Before installation, verify that all components are in good condition and that you have the necessary tools.
Choose an installation location that represents the average airflow conditions in your system.
Securely mount the air flow meter in the chosen location, considering factors like vibration and accessibility.
Connect the wiring according to the manufacturer's instructions, ensuring proper electrical connections.
Calibrate the meter to account for variations in temperature, pressure, and other environmental factors.
Perform thorough testing to ensure accurate readings, and validate the meter's performance.