You probably do not come from: United Arab Emirates. If necessary, change to: United States

Spotted: ifm and dinosaurs?!

2/27/19

In China (Beijing), Depia Automation's dinosaur show presents life-size dinosaurs impressing the audience by means of automation technology. Among others, sensors from ifm are used.

The audience has been convinced: All shows in the National Indoor Stadium (capacity: 20,000) were sold out.

In the show, dinosaurs walk, eat, fight, sleep and do many other things.
All in all, the show features twelve completely automated hydraulic "animals".

Position monitoring etc. is done, for example, by ifm sensors. More than 800 sensors are being used; of course, not all are from ifm. As Depia Automations states: "Using a mix of the best brands like Siemens, ifm, HAWE Hydraulik, Scanreco, ABB, SICK we could only succeed...". 30 high-speed PLCs and 1000 synchronised robot movements are combined using robust RFID technology.

A special SCADA system* helps to monitor and control the 40-minute automated scenario.

In the background, a 6000 sqm HD screen is used to accentuate special effects.

Have a look behind the scenes:

About Depia Automations
Depia Automations has extensive know-how about animatronics and designs automated solutions to make animatronic figures, e.g. animals, as lifelike as possible. Animatronics are used on big stages, in films, for parades, at the circus and for exhibitions of any kind.