You probably do not come from: United Arab Emirates. If necessary, change to: United States

Demand-oriented maintenance saves costs

Mining industry
Industrial communication
AS-Interface
Monitoring and maintenance
Condition monitoring
Case Study

Automated lubrication system for 1,000 kilometres of transport infrastructure

Remote maintenance
over long distances

Early maintenance alarm

Save money through demand-oriented
maintenance and reduced downtime

Results

  • Higher uptime thanks to automated lubrication
  • Manual maintenance significantly reduced
  • Early alarm in case of low lubricant levels
  • Very high downtime costs are reliably avoided

The challenge

The products are transported by a large overland conveyor system. The belt systems must always be well lubricated to ensure smooth operation of the conveyors. In the past, the mechanical lubri­cation systems featured non-electronic valves and mechanical timers, applying lubricant to the components at regular intervals of a few hours.

Lubrication occurred regardless of whether this was necessary or not, risking over- or under-lubrication of the system. An employee had to check the lubricant level at regular intervals, dri­ving many kilometres along the conveyor each time. To avoid these disadvantages, they were looking for an automated and monitored system.

Our customer

A tier 1 iron ore miner operates an inte­grated system of many iron ore mines and processing hubs. Before the ore is trans­ported further, it is crushed, processed and mixed to produce high-grade hema­tite lumps and fines.

A transport infrastructure connects the entire system to their port facilities, from where the ore is shipped to all points around the globe. The mining industry, which remains Australia’s single larg­est sector, has traditionally been slow to adopt new technologies.

Our customer

A tier 1 iron ore miner operates an inte­grated system of many iron ore mines and processing hubs. Before the ore is trans­ported further, it is crushed, processed and mixed to produce high-grade hema­tite lumps and fines.

A transport infrastructure connects the entire system to their port facilities, from where the ore is shipped to all points around the globe. The mining industry, which remains Australia’s single larg­est sector, has traditionally been slow to adopt new technologies.

The solution – why ifm?

Our customer has launched a project as a way of differentiating themselves from their compe­titors. As part of this project, an automated lubri­cation system was to be implemented to reduce manual maintenance efforts to a minimum. The new system was to dispense the lubricant only when needed.

Looking for a suitable automation solution, they decided to work with ifm. One of the main rea­sons behind this decision was that ifm offered the ‘full package’ unlike other suppliers, who, for example, were able to provide a control system but no matching sensors. ifm’s solution is based on a SmartPLC with integrated AS-Interface Ethernet/IP gateway, to which all components are connected. It came with all the required accesso­ries, such as power supply units and cables.

Especially the AS-i system integration is a major advantage for them, as it makes it relatively easy to reliably connect the devices despite the long distances. The new solution allows to record vari­ous data such as the number of cycles of the conveyor lubrication system. In addition, it mea­sures the speed of the conveyor to make sure that lubrication only takes place when needed.

The SmartObserver software is used to record the essential parameters and report them to hig­her-level systems. In addition, an alarm is trigge­red when the lubricant supply in a container is running low. The new solutions helps to avoid unplanned downtimes that would cause costs in the single-digit million-euro range.

Case Study: Demand-oriented maintenance saves costs

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.