- O6D laser distance sensor
- Applications
O6D laser distance sensor: Applications
Reliable detection and precise distance measurement are essential in nearly every industry — from metal forming to packaging and logistics. The O6D laser distance sensor delivers accurate, consistent performance regardless of target material, color, or surface condition. Using advanced time-of-flight laser technology, it provides up to 3 meters of sensing range, enabling flexible installation and dependable detection even at steep angles or in harsh environments.
Explore how the ifm laser distance sensor enhances performance across various applications below. Or read about common use use cases spanning several industries.
Sheet metal is fed into a stamping press to a certain position. The sheet metal needs to be detected that it is in position to avoid making scrap or worse, damaging the die. It does not matter if the sheet metal is stainless or mild steel, oil on the metal or not, plus it can be detected at a steep angle with the O6D sensor. Mount the sensor out of harms way and point the laser precisely where you need to detect the sheet metal coming into the die. 3 meters of range in the sensor gives you the flexibility to mount wherever you want.
Metal fabrication and forming requires position detection of various types of metals in various stages in the manufacturing process. Measuring the diameter of a large roll tells the plant when to begin the changeover process for more raw materials. Coils of wire are also easily detected with the O6D technology.
The flow of product in a warehouse distribution center is carefully controlled to optimize the automated system. Long range detection is needed to cover more ground. The product that needs to be detected to optimize the flow of the operation can be black or white; it can be a tote, box or bag. These products can also be presented in any orientation to a sensor. The O6D accomplishes all of these challenges at a distance of up to 3 meters.
A common challenge in logistics automation is being able to detect where the products are located after a stretch wrapper. Typically, retro-reflective photoelectric sensors are used. The challenge becomes the stretch wrap can “polarize” the light coming from the sensor. This makes the sensor think it is hitting its reflector, but it is not. A false non-detection occurs. The optical performance of the O6D takes away this challenge and removes the reflector from the application.
Boxes, bags and totes can be used in any distribution facility. These products turn in any direction as they move along the conveying systems. Position detection sensors need to be able to accommodate these steep angles and reliably sense the product. The O6D uses unique time-of-flight technology along with high excess gain features to achieve peak performance.
The tire manufacturing process consists of calendaring, extruding, tire building and inspection steps. During each step, the color and texture of the tire can be different. The O6D detects a dense black tire at 3 meters the same as a more “green” tire further upstream in the manufacturing process. One sensor can be used for position detection across the entire plant.
High speed assembly machines are tasked with handling very small parts. These parts can be any color and made from any material. Positioning sensors are used in these automated cells to assist with production. These sensors need to be versatile, fit into small spaces, and detect small parts. The O6D technology is the perfect solution for these applications.
Small targets need to be detected in assembly machines to ensure that all the manufacturing steps are done correctly. Small targets also mean that sensors need to fit into small spaces on the machine. The O6D has a small rectangular housing that will fit. In addition, the O6D’s ability to detect any color target at any angle provides the superior solution.
Packaging machines are constantly fed different colored labels to apply. Position sensors are used to detect labels and the final packaged good. The O6D time-of-flight laser measurement treats all colors the same, so you never have to make adjustments on the machine. If the finished good is in a bag or box, the same O6D will detect the target on the out-feed of the machine.
Production lines that run multiple parts or SKUs lose efficiency due to optical sensor misreadings or additional downtime for sensor recalibration halting operations. Planned downtime and correcting inaccurate readings halt operations.The O6D laser distance sensor from ifm overcome these challenges with continuous, automatic recalibration and patent-pending time-of-flight technology.
Production environments expose optical sensors to dust, moisture, oil mist, and other irritants. Lighting conditions often change throughout the day. These harsh or changing environmental conditions degrade optical sensor performance. They cause unreliable readings resulting in false positives and missing objects completely The 06D uses laser point detection and continuous recalibration to avoid interference and account for changing conditions.
Production lines handling multiple materials lose efficiency due to missed detections and false triggers from optical sensors. These problems are common when objects with very different shapes, colors, or textures come down the same line, sometimes less than a second apart and closer than one inch to each other. overcomes these common challenges with new automatic recalibration technology.
Manufacturing equipment creates physical barriers that limit where optical sensors can be mounted. Sensors that are too far, too close, or at the wrong angle become unreliable, leading to missed detections, false positives, or complete detection failure as products move through the line. The O6D uses a point laser beam and time-off-flight technology to overcome common mounting constraints that impact detection.