• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. O6D laser distance sensor
  2. Technology

O6D laser distance sensor: Time-of-flight technology

Common CMOS-based distance sensors use the triangulation operating principle. When mounting restrictions require these sensors to be mounted at an angle, insufficient light from the target is reflected back to the sensor to determine the distance.

The O6D time-of-flight principle does not rely on triangulation. When light bounces off the target, the phase pattern of the transmitted light shifts and the shift is directly proportional to the distance. The sensor only requires a small amount of reflected light to accurately determine the distance.

Choose an O6D sensor for your application

 

Advantages of time-of-flight measurement:

Browse all laser distance sensors from ifm.