• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • my ifm

Automotive manufacturing: Stamping press monitoring and predictive maintenance with moneo

Automotive
Press shop
Steel and metal industry
Application report

Stamping presses are critical assets often used to manufacture automotive components.

How the moneo IIoT software platform enables real-time monitoring and predictive maintenance of stamping presses

The manufacturer wanted more insight into the condition of their stamping presses to better inform their maintenance program. Implementing a full ifm solution provided immediate business impact and transitioned the maintenance program from a preventative to a predictive schedule. 

Benefits

Reduced unplanned downtime Enabled predictive maintenance Reduced production costs

Estimated savings

Prevented $500,000 in maintenance costs and 5 weeks of press downtime.

Based on a 20% chance of a catastrophic failure and associated costs of a press rebuild, the investment achieved an estimated Return On Investment (ROI) in just 2.5 months.

ifm has very knowledgeable employees that continue to work with our engineering and maintenance teams to help better our processes and expand on their understanding of our equipment and needs. The ifm team is accepting to all input from our team and finds a way to make our requirements their tasks.

Automotive supplier ifm Customer

About the customer

They are a Tier 1 supplier of metal assemblies for the global automotive industry. They proudly provide metal components for over 50 vehicle models in North America. 

ifm has very knowledgeable employees that continue to work with our engineering and maintenance teams to help better our processes and expand on their understanding of our equipment and needs. The ifm team is accepting to all input from our team and finds a way to make our requirements their tasks.

Automotive supplier ifm Customer

About the customer

They are a Tier 1 supplier of metal assemblies for the global automotive industry. They proudly provide metal components for over 50 vehicle models in North America. 

Project Goal

Optimize maintenance plans

The automotive supplier was looking to rebuild a large transfer press that had a handful of mechanical issues. A full rebuild of a press this size is extremely costly and time-consuming. They partnered with ifm to implement a condition monitoring system on the stamping press that would alert the team if mechanical issues occurred after the rebuild. To ensure centralized data collection, the project had a requirement of interoperability with all existing IT infrastructure, including SCADA and CMMS.

Simpify implementation

To evaluate the speed of deployment fairly, the customer decided to start the implementation of data monitoring dashboards simultaneously using two different platforms. The customer started the moneo implementation at the same time as they initiated the process of creating the dashboards through their internal IT team within the existing SCADA system. 

Stamping press maintenance challenges

Mechanical stamping presses are commonly used in aerospace, automotive, and appliance industries. Large presses are expensive to replace and maintain but are uniquely suited for heavy-duty metal forming due to their accuracy and versatility in high-speed, high-volume production. Because of the size and complexity of these machines, various assets on the press are susceptible to significant downtime events, including motors, flywheels, bearings, and linkages.

With significant production demands, even preventative maintenance is difficult to schedule. The customer needed to gain visibility into machine conditions and alert to impending failures, in order to optimize maintenance plans before they occurred during production. Whether planned or unplanned, stamping press downtime leads to:

  • Weeks or months of lost production revenue
  • Just in Time (JIT) production penalties
  • Outsourced production during maintenance
  • Maintenance and labor costs of reconfiguration

While downtime for maintenance reduces production time, catastrophic failures of equipment result in months of downtime and outsourcing of production until the root cause is identified and fixed. Ongoing maintenance of stamping presses is required to ensure presses remain operational. Many companies complete maintenance based on timed intervals or by the number of unplanned stops, but these are usually not determined by machine data.

With improved insight into machine conditions in real time, the customer would also be able to verify that presses were set up correctly before restarting production.

Simplifying implementation

One licensed engineer installed the VSE vibration edge controllers, 8 IO-Link masters, and accelerometers. The entire hardware and software implementation took a few hours, and they started trending sensor data to customized dashboards in just one day. The initial setup focused on vibration monitoring of the stamping press, and later expanded to include real-time monitoring of:

  • Motor and gear assembly
  • Compressed air
  • Linkage and bearing condition
  • Lubrication quality

Results

At this point, the IT engineer decided to stop the SCADA system integration. It would still take weeks to implement the same visualization and data analysis as achieved in the moneo IIoT software platform through their existing SCADA system. This test determined that implementing moneo reduced implementation time from weeks to hours. 

Optimizing maintenance with real-time data

Within the first month, the engineering team received an alert in moneo that a linkage in the left corner of the press was 20 °F higher than the other corners of the press. When the maintenance team investigated, they discovered that the die was not mounted in the middle of the press. By favoring the left side, the counterbalance could not support the weight and extra load, resulting in an overheated bushing. Off-center loading is a major press issue that is difficult to detect, but moneo helped to proactively catch the problem and avoid an estimated $500,000 in maintenance costs and 5 weeks of downtime.

 

Due to the plug-and-work principle of ifm sensors and embedded IO-Link technology, it is simple to add new data sources to production and collect that data in the moneo IIoT software platform. All ifm IO-Link sensors can be parameterized using the free moneo configure software download, but those with an active moneo licensed subscription will find it conveniently accessible from their full software suite homepage. Reducing integration and installation time makes asset monitoring simple and easy. 

Conclusion

The initial installation provided immediate results in the first two months, verifying the ifm approach of proving value of a predictive maintenance project as quickly as possible. This approach helped the customer by:

  • Optimizing maintenance plans with visualizations of diagnostic data 
  • Reducing complexity with intuitive hardware and software
  • Simplifying implementation without IT development

The customer verified that the concept worked for the stamping press application before investing significant time or capital expenditure into a new technology stack. With machine health dashboards created in hours, the engineering team could immediately visualize and gain insight into the status of the stamping press. The interoperability of ifm sensors and the moneo IIoT software platform simplified the transfer of data to SCADA and CMMS systems without interfering with production operations. Ultimately, the customer implemented the solution and proved business impact within just a few months, showing how simple it is to get started. 

 

Explore the moneo IIoT software platform
Want to get started?

If you would like to discuss your application, please contact our solution team. Our engineers are here to help.

Explore more solutions for the automotive industry