• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. Calibration services
  2. Calibration verification certificates | vibration

Calibration of vibration sensors

ISO calibration of vibration sensors

The comparative measurement of vibration sensors is carried out by comparing the measured value of the transducer to be calibrated with that of a standard accelerometer.

The sensor to be calibrated and the reference sensor are mounted on a sandstone table and set to a sinusoidal oscillation in a defined frequency range. In addition to the zero point, calibration is carried out in the frequency range between 20 Hz ... 800 Hz with a constant vibration velocity of 10 mm/s at 11 measuring points from the one-third octave range.

Calibration is performed via the analog output (current) as standard in the factory setting.

Calibration verification certificate for vibration sensors VTV/VKV (Part no. ZC0116)

  • Fee charged.  One certificate per sensor required.
  • Generated by ifm's calibration lab.
  • Applies to the specified article(s) and must be ordered with the sensor.  It cannot be generated after the sensor has been delivered.
  • For new purchases only. We do NOT offer recalibration services for sensors that have been in service.
  • Only available for VTVxxx and VKVxxx vibration sensors.