• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm

P|Prox displacement sensor: Extreme precision measurement for all metals

 

The IxP precision proximity sensor (P|Prox) family performs the work of a traditional displacement sensor at a fraction of the price in industries such as automotive, factory automation, food & beverage, machine tools, and metalworking.

The state-of-the-art technology enables reliable operation even when exposed to high magnetic fields. The P|Prox proximity sensor, with excellent repeatability, ensures process stability and improves product quality by measuring absolute distance values between the active sensing face and a metallic target directly in pure digital form.

The inductance change is measured and converted into an absolute distance value in the microcontroller without A/D conversion losses. This allows the sensor to provide sub-micron resolution. Accuracy and repeatability remain constant regardless of the target metals.

Benefits

   
Improve process stability and product quality   Reduce total cost of ownership   Simplify complexity
  • Extremely high accuracy in the micrometer range ensures most precise process control and yields products with the best quality.
  • Unparalled repeatability! Process drift due to unstable or inconsistent measurements is elimiated, ensuring the same quality level for each batch.
  • Pure digital IO-Link output without conversion loss provides no negative impact on the actual measured value.
 
  • Commissioning costs are reduced since no manual scaling is required. The P|Prox outputs the absolute distance to a metallic surface in mm continuously.
  • Reduce inventory costs, since one sensor provides accurate distance measurement of all types of metal. No correction factor is required.
  • Standard M8, M12, M18, and M30 form factors eliminate the need for special mounting and calibration accessories.
 
  • Plug-and-work on all metal targets, elimiating time-consuming fine adjustment.
  • One-piece design with compact housing without the need of an external evaluation unit.
  • Factory calibrated with aluminum provides best performance on all metals.
  • If necessary, immediate performance improvement can be achieved with 1-click on-the-fly calibration.

Traditional analog sensor

P|Prox displacement sensor with IO-Link

 

Accuracy and repeatability vary

  • Factors such as thermal noise, signal attenuation, temperature, and other influences affect negatively affect analog signals.
  • Degradation of analog signals lead to toss of information and reduced measurement accuracy.
 

State-of-the-art technology provides sub-micron accuracy and repeatability

  • P|Prox measures the distance to the target and directly converts this measurement into a digital distance value within its microchip.
  • Minute changes in distance can be measured and signaled. No internal conversion losses provide consistent accuracy and repeatability.
  • Low temperature drift.
 

Time-consuming adjustments, calibraion, and manual scaling

  • Applications requiing high resolution measurements often require time-consuming on-site calibration.
  • Mechanical fine adjustments using spacers is usually performed after the sensor is installed.
  • Analog signal is proportional to the measured distance and manual scaling is generally required.
 

Plug-and-Work solution

  • Since the output is absolute distance in mm, no manual scaling is required.
  • Default calibration is done with aluminum.
  • Standard performance, acceptible most applications, is achieved with other metals such as steel, and stainless steel
  • For specialty applications such as detection of small objects, calibration can be done in seconds.
 

One sensor for one type of metal

  • Traditionally, to achieve high accuracy, the application is target-dependent and the sensor is calibrated for one type of metal.
  • For other metals, a new sensor custom calibration is required.
 

One sensor for ALL metals

  • No reduction in range, and accuracy and resolution of distance measurement are constant with all metals.
  • Simplifies the integration and reduces inventory complexity.
 

No additional diagnostics

  • Traditional inductive sensors only output discrete or analog signals that are susceptible to noise interferences.
  • Connection requires long home run cables or direct connections, often with hundreds of wire terminations.
  • Information on sensor health and application strength is not available.
 

Unlock the power of IO-Link

  • Information such as real-time alerts and reactions, device temperature, and other device diagnostics are available.
  • P|Prox connects to an IO-Link master via an industry standard M12 A-coded cordset.

Explore the features