- SDP gap distance sensor
- IO-Link benefits
SDP Gap distance sensor: IO-Link benefits
Through IO-Link, the SDP air gap sensor can provide:
- Current gap measurement in µm
- Current air flow rate and system pressure
- Output and device status
- Automatic device replacement
Easy setup using IO-Link "Teach" function
Due to ever smaller batch sizes, it is constantly necessary to teach in new workpieces or new production positions. To teach in the switch point, predefined gauges or patterns defined as good parts are placed in the machine. The sensor is set to the corresponding distance value.
To reduce short stops associated with changeovers, setup must be accomplished efficiently and quickly. Where conventional sensor technology requires time-consuming adjustment via buttons on the sensor, the SDP gap sensor offers the option of teaching in switch points conveniently and at the touch of a button either via the integrated IO-Link interface or via the separate teach input. This reduces the set-up time considerably.
More benefits of air gap sensors with IO-link connectivity
Integrating IO-Link connectivity with air gap sensors enhance the performance, reliability, and efficiency of modern industrial processes. Here's how IO-Link revolutionizes the application of air gap sensors:
Improved product quality
The transition from analog to 100% digital communication with IO-Link ensures more reliable and accurate data transmission. This precision contributes significantly to enhancing product quality by enabling predictive maintenance and ensuring the consistency of the manufacturing process.
Lower operational costs
IO-Link connectivity simplifies the system architecture by eliminating the need for analog input cards. This can lead to smaller control cabinets and reduced wiring complexity. The streamlined setup results in substantial installation and maintenance cost savings.
Increased production efficiency
IO-Link facilitates rapid recipe changes through its bidirectional communication capability, allowing seamless interaction between the air gap sensors and the higher-level control systems. This agility in adapting to new production demands greatly enhances operational efficiency.
Enhanced machine uptime
In the event of a sensor replacement, IO-Link automatically configures the new sensor with the parameters of its predecessor, significantly reducing downtime and accelerating the resumption of production activities.
Comprehensive monitoring
Get detailed real-time data, including the current gap measurement in micrometers, airflow rate, system pressure, and the status of both the output and the device itself.