• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain
  • my ifm
  1. IO-Link signal converters
  2. Select products
  3. Pulse extender

Pulse Extender

In processes with short switching pulses, it is a challenge for the control system to reliably detect every single switching pulse of a sensor. The DP2402 and DP4402 converts every input pulse, no matter how short, into a switching signal with a defined duration. In addition, a delay time can be set for the output of the switching signals.

The DP2402  and DP4402 can be connected directly to a sensor with an M12 connector and can also be used directly in the field thanks to its high IP protection. This saves valuable space in the control cabinet.