• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. O6 small rectangular photoelectric sensor
  2. Setup and support
  3. Device configuration

O6 Photoelectric sensors: Device configuration

The following will guide you through key programming steps for the O6 sensors. We highlight the features used most often here. Refer to the Operating Instructions manual found under the “Downloads” tab at the product datasheet page for more details on programming the sensors and other features.

You can also visit our installation instructions or FAQs page. Should you need additional support, feel free to contact our service center at 1-800-441-8246 and speak to one of our applications engineers.

Operating and display elements

 

  1. Yellow LED - output switched on
  2. Sensitivity adjustment potentiometer
  3. Green LED - power on / stability indication
  4. Output selector

Note: The through-beam transmitter features only a green LED to indicate power/operational status.

Stability indication

The green LED is lit when supply voltage is applied and there is enough excess gain from the application. The table below indicates the behavior of this LED.

Setting the sensitivity

  • To increase sensitivty, turn the potentiometer (2) clockwise.
  • To decrease sensitivity, turn the potentiometer (2) counterclockwise.

Setting the output function

  • For dark-on mode (output turns on when no light reaches the receiver), turn the potentiometer (4) to “D”.
  • For light-on mode (output turns on when light reaches the receiver), turn the potentiometer (4) to “L”.