• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. IO-Link vibration monitoring
  2. Applications and installation

VVB IO-Link vibration sensor: Applications

ifm’s VVB vibration sensor is used for permanent, real-time monitoring of vibrations in simple industrial machinery. Even minimal deviations from the ideal machine condition will affect the vibration pattern. This makes it possible to detect imminent machine damage at an early stage. Plant operators can act with foresight and anticipate maintenance needs to avoid costly production downtimes.

Measurements and monitoring methods

The VV design aims to simplify the primary categories of machine failure. Unlike typical single measurement systems, the VV vibration meter simultaneously monitors equipment for the five categories of machine problems: impact, fatigue, friction, severity, and temperature. The embedded IO-Link technology provides this data in real time, giving the VV sensor the capability to predict pending failures and mitigate catastrophic damage.

Example fault
conditions
Blades hitting
Ingested object
Struck by moving object
Improper sequence timing
Misalignment
Unbalance
Belt issues
Loose footing
Structural issues
Failing bearing
Rubbing impeller
Dragging blade
Cavitation
Damaging condition
Instability
Loss of lubrication
Loss of coolant flow
Electrical issues
Excessive load
Fault category Impact
Crashes
Striking
Fatigue
Mechanical issues
Assembly issues
Friction
Rubbing
Grinding
Severity
Uncontrolled forces
Impulses
Temperature
Over heating
Sensor measurement Acceleration peak
(a-Peak)
Average velocity
(v-RMS)
Average acceleration
(a-RMS)
Crest factor
(a-Peak / a-RMS)
Degrees Celsius
(C)

The crest factor is a leading indicator of damaging fault conditions. It measures the severity of impacts relative to the normal operating state of the machine. It filters out the influence of rotational speed to simplify setting alarm limits.  Crest factor values in the 4...8 range indicate potential machine problems.

Sensor mounting location installation guideline

Typically, we recommend mounting sensors radially to shaft rotation to detect the greatest level of movement and located mechanically as close to the target as possible. The orange dots in the images indicate approximate sensor location for smaller machines. If the mounting location is greater than 80 cm (30+ inches) apart, we recommend adding additional sensors as shown by the grey dots in the images.

Note: All sensors are capable of measuring all alarm conditions and identifying root causes. 

Axial fan

Machine No. of sensors Sensor location   Alarms Root issue

Axial fan

Primary: 1

Optional: 1

Radial H-DE motor

Radial V-NDE motor

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, DE = driven end  

It is suggested that mounting locations greater than 80cm apart also use the optional location.

 

Radial direct drive fan

Machine No. of sensors Sensor location   Alarms Root issue

Radial direct drive fan

Primary: 1

Optional: 1

Radial H-DE motor

Radial V-NDE motor

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, V = vertical, DE = driven end, NDE = non-driven end 

It is suggested that mounting locations greater than 80cm apart also use the optional location.

 

Radial indirect drive fan

Machine No. of sensors Sensor location   Alarms Root issue

Radial indirect driven fan

Primary: 1

Primary: 1

Optional: 1

Optional: 1

Radial H-DE motor

Radial V-DE fan

Radial V-NDE motor

Radial H-NDE fan

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, V = vertical, DE = driven end, NDE = non-driven end 

It is suggested that mounting locations greater than 80cm apart also use the optional location.

Centrifugal pump

Machine No. of sensors Sensor location   Alarms Root issue

Centrifugal pump

Primary: 1

Primary: 1

Optional: 1

Optional: 1

Radial H-DE motor

Radial H-DE pump

Radial V-NDE motor

Radial V-NDE pump

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, V = vertical, DE = driven end, NDE = non-driven end 

It is suggested that mounting locations greater than 80cm apart also use the optional location.

Electric motor

Machine No. of sensors Sensor location   Alarms Root issue

Electric motor

Primary: 1

Optional: 1

Radial H-DE motor

Radial V-NDE motor

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, V = vertical, DE = driven end, NDE = non-driven end 

It is suggested that mounting locations greater than 80cm apart also use the optional location.

Speed reducer

Machine

No of
sensors

Sensor location   Alarms Root issue

Speed reducer

Primary: 1

Optional: 1

Radial H-DE reducer

Radial V-NDE motor

 

a-Peak

v-RMS

a-RMS

Temp

Impact

Looseness

Friction (bearing)

Overheating

Legend:  a = acceleration, v = velocity, H = horizontal, V = vertical, DE = driven end, NDE = non-driven end 

It is suggested that mounting locations greater than 80cm apart also use the optional location.

When applying real-time continuous monitoring, 3-axis measurements are typically not needed. 3-axis techniques are typically used in traditional route-based analysis methods where only a snapshot of the machine health is recorded. In some cases where machine design implements axial loading, a second axial sensor may be necessary.

For a more detailed comparison of single-axis vs. multi-axis measurements, please visit our technology page.