• Products
  • Industries
  • IIoT & Solutions
  • Service
  • Company

Moneo: your actionable insights dashboard

Moneo is a dashboard and analysis tool which converts sensor data into actionable information allowing you to closely monitor your factory or plant to avoid downtime and increase your productivity.

Moneo is industry-independent, manufacturer-independent IIoT platform and thus enables you to integrate a wide range of existing devices and use the data more efficiently.

What can moneo do you for me?

Data visualisation is not the only capability of Moneo. Our full package allows you to do all of the following:

  • Monitor live values from machines.
  • Create Dashboards or Overview status pages.
  • Create alerts from machine data and/or insights.
  • Create calculations or metrics across multiple machines.
  • Create quick time series graphs/comparisons across multiple machines.
  • Simple data exports (by csv) of machine sensor data or insights.
  • Process and translate machine data and send to IT systems or Cloud.
  • DataScience integration to provide automated insights/alerts based on exceptional machine data.
  • Integration into SAP possible.

At Sheard Packaging we are always looking at way to make our production smoother, faster and more cost efficient. As part of this we work closely with ifm to implement new technologies to revamp and monitor our most crucial equipment.

Working together we have been able to think outside the box and come up with new methods to achieve this using cutting edge technology from ifm including moneo Vibration Analysis that allows us to plan our maintenance and greatly reduce our unplanned Downtime.

Dean Sherman
Electrical Maintenance Manager
Sheard Packaging

How does moneo work?

For over 50 years, we have been supporting our customers as a leading supplier of automation solutions. We have now combined our experience in sensor technology with the expert knowledge of our software subsidiaries – this is moneo, "simply made for you".

How will moneo benefit me?

Make better informed decisions

Moneo makes your plant more efficient.  With moneo, machines can be maintained predictively and unplanned downtimes can be avoided. 

Go at your own pace

The function modules are scalable for all machines. The moneo starter kit is the perfect start into digitisation. If you are ready for the next steps, an extension by further modules or device connections is easily possible. With the infopoint licences, the costs depend on the number of data points that are in use.

Further modules are being planned and implemented. These expand the moneo portfolio.

Avoid downtime

Moneo analyses the sensor data and detects deviations. If a machine is running differently than usual, this indicates wear or changes in the process that could lead to a failure.

There is often enough time between the occurrence of the first deviations and a standstill to schedule predictive maintenance.

 

What are the advantages of having moneo?

Simplified integration

Moneo has a user-friendly interface and makes it simple and fast to implement modules.  Thus, your IIoT project will be immediately ready to go.

Low up-front costs and very high flexibility

The modular approach of moneo is particularly flexible in adapting to the requirements of an IIoT project for different applications and industries. You can book the moneo modules as required. This offers convenient use with low investment costs and very high flexibility. For smaller projects, a starter kit pack is also available.