• Products
  • Industries
  • IIoT & Solutions
  • Service
  • Company

What is a proximity sensor used for?

A proximity sensor detects the presence, absence, or movement of an object without physical contact. In industrial environments, these sensors are used to automate processes, prevent collisions, trigger machine operations, and enhance safety and efficiency across production lines.

What are the four types of proximity sensors?

The four main types of proximity sensors commonly used in industrial settings are:

  1. Inductive sensors – Detect metal objects using electromagnetic fields.

  2. Capacitive sensors – Detect both metallic and non-metallic objects (e.g. plastic, glass, wood) by sensing changes in capacitance.

  3. Ultrasonic sensors – Use sound waves to detect objects, regardless of material, shape, or colour.

  4. Photoelectric sensors – Use light beams to detect objects, including transparent or reflective materials, over longer distances.

Each type is suited to specific applications based on the target material, sensing distance, and environmental conditions.

What is a PNP and NPN proximity sensor?

PNP and NPN refer to the type of transistor output used in the sensor’s wiring, which determines how the sensor connects to a control system:

  • PNP (sourcing): When an object is detected, the sensor outputs a positive voltage. Commonly used in Europe.

  • NPN (sinking): When an object is detected, the output is pulled to ground (0V). Commonly used in Asia.

Key difference:

  • In PNP, current flows out of the sensor to the input of the controller.

  • In NPN, current flows into the sensor from the controller.

Selecting the correct type depends on your PLC or controller input configuration. For example, the IFM203 inductive sensor supports both PNP and NPN configurations.

What is the sensing range of an industrial proximity sensor?

The sensing range refers to the maximum distance at which a sensor can reliably detect an object. This varies by sensor type, material of the target, and environmental conditions.

For example, IFM inductive proximity sensors offer sensing ranges from as short as 2 mm (compact models) to 120 mm (long-range models). Actual performance may vary depending on the target’s size, shape, material, and conditions such as temperature and humidity.

Choosing a sensor with the right sensing range for your application is key to ensuring accurate, reliable detection.

How do proximity sensors work?

Proximity sensors detect objects without making physical contact. They trigger a signal when something enters their detection zone. Different types of proximity sensors use different principles:

  • Inductive: Use electromagnetic fields.

  • Capacitive: Use electric fields.

  • Ultrasonic: Use sound waves.

  • Photoelectric: Use light beams.

All are designed for reliable, non-contact detection—ideal for automated machinery and systems.

Examples of proximity sensors and their uses

1. Inductive proximity sensors

What they detect: Metal objects
How they work: Use magnetic fields to detect metal
Where they’re used:

  • Robot arms and machinery for position detection

  • CNC tools to confirm metal part placement

  • Harsh environments such as welding stations
    Best for: Reliable metal detection in dirty or wet conditions

2. Capacitive proximity sensors

What they detect: Both metal and non-metal materials
How they work: Use electric fields to sense changes in capacitance
Where they’re used:

  • Detecting plastic, glass, wood, or liquids

  • Level detection in bins or tanks

  • Sensing through packaging or non-metal containers
    Best for: Versatile detection of solids and liquids

3. Ultrasonic proximity sensors

What they detect: Any object, regardless of material
How they work: Emit sound waves and detect the returning echo
Where they’re used:

  • Measuring liquid levels, even with foam

  • Object detection for automated vehicles

  • Detecting transparent or oddly shaped objects
    Best for: Detecting difficult-to-see or irregularly shaped targets

4. Photoelectric proximity sensors

What they detect: Objects that interrupt or reflect a light beam
How they work: Use light (laser or LED) to detect interruptions
Where they’re used:

  • Counting items on conveyor belts

  • Checking for labels on packaging

  • Detecting small components in electronics
    Best for: Long-range or high-speed object detection

What is the difference between inductive and capacitive sensors?

Inductive sensors

  • Detect: Metallic objects only

  • Operating principle: Generate an electromagnetic field; detection occurs when a metal object disrupts it

  • Applications: Position sensing, gear detection, metal counting

  • Advantages: Robust performance in dirty, oily, or wet conditions

  • Limitations: Cannot detect non-metallic materials

Capacitive sensors

  • Detect: Metallic and non-metallic materials (e.g. plastic, powder, liquids)

  • Operating principle: Generate an electrostatic field; detection occurs when an object changes the field’s capacitance

  • Applications: Liquid/solid level detection, packaging lines

  • Advantages: Broad material detection, can sense through container walls

  • Limitations: Sensitive to humidity, temperature; may require calibration

Choosing the right sensor:

  • Use inductive sensors for reliable metal detection in tough environments

  • Use capacitive sensors for detecting a variety of materials or for sensing through surfaces

Do inductive sensors only detect metal?

Yes, inductive sensors are designed to detect metals only. They function by emitting an electromagnetic field, which is disrupted when a metal object enters the sensing zone.

  • Ferrous metals (e.g. steel, iron) are most responsive.

  • Non-ferrous metals (e.g. aluminium, copper, brass) can be detected but usually at reduced ranges.

However, IFM’s Kplus series of inductive sensors overcome this limitation. With a correction factor of 1 (K=1), they detect both ferrous and non-ferrous metals at the same distance, reducing the need for sensor variations or recalibration.

Additionally, ferrous-only sensors are available for applications like machining, where aluminium chips could otherwise trigger false signals. These are tuned specifically to ignore non-ferrous materials.

For product specifications, environmental guidance, and application tips, visit:

🔗 IFM Inductive Sensors – Product Range
🔗 IFM Capacitive Sensors – Product Range