• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • Supply Chain Software
  • my ifm
  1. LDH oil humidity sensor
  2. Setup and support

LDH Oil humidity sensor: Installation guidelines

Thank you for purchasing the LDH oil humidity sensor. On the following pages, you will find information to help you quickly install the humidity sensor as well as answers to frequently asked questions. For more details, please refer to the operating instructions with the product datasheet.

Should you need additional support, feel free to contact our service center at 800-441-8246 and speak to one of our application engineers.

Typical measuring system

To accurately measure oil condition, humidity sensors should be installed in a representative position, such as in the return flow. Ideally, place an LDH oil humidity sensor in the tank near the return pipe. Alternatively, it can be installed in the rinse pipe if there are interferences like gears with forced rinsing.

  1. Connection of the return pipe
  2. Pipe lengthwith unit*
  3. Consumer
  4. Pump
  5. Connection of the rinse pipe
  6. Unit directly screwed into the tank wall

*The pipe length may consist of a pipe section of a suitable diameter.

Important sensor placement for operation

To properly install the LDH oil humidity sensor, ensure the sensor probe is fully submerged in the measured medium and placed where there is consistent flow around the sensing element to prevent dry running and potential damage. Mount the unit below the minimum oil level in all operating conditions and away from heat sources such as motors to avoid thermal interference.

  1. Wrong installation position
  2. Minimum oil level in the tank
  3. Connection of the return pipe
  4. Connection of the rinse pipe
  5. Sensor vertically installed in the bottom*
  6. Horizontally installed sensor
  7. Installation angle

*Note possible formation of layers or sediment

If installing the sensor in a lower position within an oil tank, ensure the oil is sufficiently mixed to prevent stratification (layers of oil with different saturation levels).

 

When installing the unit in a return or rinse pipe, maintain consistent flow around the sensing element to prevent dry running in any operating condition.

 

Ensure the measuring element is fully submerged in the oil, taking into account potential variations in tank level or tilted positions during installation.

Installation procedure

LDH112 (G1/2): Check profile sealing ring (A) for correct position (in a groove).
LDH122 (1/2"NPT): Apply a suitable sealing material (e.g. PTFE tape) to the thread, if required.

 

Lightly grease the thread of the unit using a lubricating paste which is suitable and approved for the application. Screw the unit into the process connection (B) and tighten firmly.

 

Maximum tightening torque:

  • LDH112: 20...25 Nm

  • LDH122: ≤ 50 Nm

Explore the full range of ifm's oil humidity sensors.