The Midvaal Water Company is a water service provider supplying potable water in bulk to South Africa, serving an area of some 900 km². Situated on the banks of the Vaal River, the company purchases raw untreated water and after purification, delivers it to consumers.
To secure the supply of drinking water, Midvaal focuses on integral pump and motor monitoring. Especially through the use of IO-Link, Midvaal was able to reduce the time required for wiring by 80 %. In addition, remote monitoring of the pump station is now possible.