Nereus integrates ifm sensors in its filtration systems to ensure their trouble-free operation and reliable function. Thanks to IO-Link, precise data is available to the company without conversion losses. In addition, the company saves a lot of time in the production process: The cabling can be implemented more quickly and without errors, and the parameter setting of the sensors takes less time. Thanks to seamless transfer of all files to the IT level, Nereus is able to monitor all installations remotely and react immediately if necessary. This significantly reduces the downtime of plants.