You probably do not come from: Namibia. If necessary, change to: United States

Ramaplast – IO-Link optimises energy generation

Other industries
Packaging industry
Industry 4.0
Networking
Video report

In the power plant owned by the company Ramaplast the primary energy gas is used to generate electricity as well as cold and heat for the production lines. Besides plant transparency the IO-Link interface in the sensors also ensures maximum efficiency.

Our customer

Ramaplast SpA is a company founded in 1973 in Italy, which operates in the field of injection moulding of rubber and plastic.

Our customer

Ramaplast SpA is a company founded in 1973 in Italy, which operates in the field of injection moulding of rubber and plastic.

IO-Link systems from ifm

Point-to-point communication with IO-Link systems from ifm

IO-Link has been developed by leading sensor, actuator and control manufacturers. The result is a standardised and fieldbus independent interface for automation. This provides the user with point-to-point connections without complex addressing. Binary switches that used to be limited to simple switching signals or analogue values have developed into smart sensors.

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.