You probably do not come from: Namibia. If necessary, change to: United States

Koedood equips the first inland vessel with hydrogen propulsion

Port automation
Ship automation
Mechanical engineering
Application report

Emission-free inland shipping

The European goods transport chain could not be imagined without inland navigation. On the contrary: Aiming to become the worlds first climate-neutral economy by 2050, the EU wants to promote inland shipping more actively as one of the most CO2-efficient transport modes. In order to significantly reduce the still quite high emissions on the over 40,000 km of navigable inland waterways, the EU focuses on clean fuel through effective after-treatment of exhaust gases and new forms of propulsion.

In both areas, Koedood acts as a competent partner. The company, which is based in Hendrik-Ido-Ambacht near Rotterdam in the Netherlands, retrofits existing ships with diesel engines that comply with the strict EU Stage V emission regulations. By developing a proprietary after-treatment system we call Koedood Engine & Emission System, or KEES, we have been able to significantly reduce nitrogen oxide emissions, says Sander Roosjen, Research and Development Manager at Koedood.

Ship on inland waterway

Modular system in 20 ft format

The K2 a reference to the two companies Koedood and Kooiman and the chemical hydrogen formula H2 is dimensioned to fit into a standard 20 ft container. It consists of 32 low-temperature PEM fuel cells, an air supply and a cooling water circuit. The required hydrogen is transported onboard the ship under low pressure.

ifm really understands our needs and what we want to achieve, and provides us with the necessary automation solutions.

Sander Roosjen Research and Development Manager at Koedood

Our customer

Koedood is a company that sells diesel engines for the inland marine sector and focuses, among other things, on the electrification of vessels in hybrid systems.

ifm really understands our needs and what we want to achieve, and provides us with the necessary automation solutions.

Sander Roosjen Research and Development Manager at Koedood

Our customer

Koedood is a company that sells diesel engines for the inland marine sector and focuses, among other things, on the electrification of vessels in hybrid systems.

Sensors ensure optimum efficiency

For monitoring and optimum operation of this system, Koedood uses various sensors from ifm, including the LMC100 point level sensor, the TA2405 temperature sensor, the PT5503 pressure sensor and the LR9020 level sensor. Because it is a completely new propulsion system, we do of course want to collect as much data as possible to ensure smooth operation of the system, says Roosjen.

60 sensors monitor the fuel cell propulsion and transmit the data to the IT level for evaluation.

To achieve optimum efficiency, all relevant process values must be precisely adhered to. So, it is important for us that the sensors are always reliable and accurate. Fresh air with a constant level of humidity must continuously be transported to the fuel cells. In addition, the operating temperature of the fuel cells must be kept at a constant level to ensure the best possible energy yield. In addition to the required energy for the ships engines and on-board electronics, pure water is produced as a by-product of the conversion. We use some of it as cooling water in the process cycle and need to ensure its availability on a permanent basis. The excess water can simply be pumped out of the cycle.

Koedood relies on ifms innovative strength

Koedoods development of a zero-emission propulsion system for inland vessels can truly be called pioneering work.

As an innovative company, we have recognised the potential of inland navigation to become an even greener mode of transport, and we want to do our part with clean propulsion solutions, says Sander Roosjen. This is why we like working with ifm as a company that continuously drives the innovative development of its sensor technology forward. ifm really understands our needs and what we want to achieve, and provides us with the necessary automation solutions. Joining forces and combining strengths and competences gets you further. And that is exactly what ifm and Koedood are doing in the case of maritime fuel cell propulsion.

Conclusion

With innovative developments, Koedood is driving the change towards clean propulsion solutions for inland navigation. The company relies on ifms technical expertise and process sensor technology to achieve maximum efficiency in their hydrogen propulsion systems.

Download application report (PDF)
What is your success with ifm?

Have you implemented an interesting application with hardware or software from ifm? How do our sensors help to optimise your process operations? Let us know! We will be happy to show your solution and present your know-how to a large audience free of charge, of course.

Increasing the efficiency of port operations

Automation and connectivity of the future

We offer targeted and safe solutions for any port application, which are aimed at precisely these requirements.

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.