ifm efector in the FABTECH Mexico Trade Show
ifm efector was present at the Expo FABTECH Mexico at Cintermex Forum in Monterrey, during May 2-4 2017.
The FABTECH Mexico Trade Show is the primary gathering for Welding, Forming, Painting and Covering Manufacturers in Mexico and this year brought 575 exhibitors to cover more than 140,000 net square feet of show floor. Over 13,000 attendees from Mexico and South America on Cintermex to find solutions, network, learn and experience first-hand the latest innovations in the metal forming, fabricating, welding and finishing industries.
This was the first time of ifm on this event with a great success, around 400 visitors on ifm's stand were those who could observe and live up to the latest news and technology that ifm efector presented in such an important event.
The new structure of the booth allowed it to present 7 different panels showing the top leading products: K-Plus, IO-Link, opto, pressure, flow, vibration and level. The IO-Link module was one of the most viewed technologies, incorporating 3 KT sensors that changed from "mode 1" to "mode 2" and "mode 3", meaning rotating all displays or changing from green to red, of all the sensors showed, at the same time.
The next big event for ifm efector will be Expo Minergy 2017, with visitors and customers from the Energy, Mining and Metallurgy Industries. See you next time!
Thank you very much to all of the ifm Mexico team for the support shown during this event!