OEE in manufacturing
The Overall Equipment Effectiveness (OEE) provides information about the degree of added value of a plant. Three factors are taken into account: the availability, the power factor and the quality factor. The goal is to increase value creation and avoid wastage. In order to give these values some content, extensive data analysis is needed. Special software is often used to collect and analyse the data.
| Availability | Power factor | Quality factor |
|---|---|---|
|
|
|
How is the OEE calculated?
- Typical manufacturers achieve an OEE of 60 to 65%.
- World class manufacturers achieve an OEE of 85%.
- An OEE value of 100 % means that the process is always running at maximum speed during the planned production time and that all parts produced are usable.