• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company

PVA TePla – Digitised single-crystal growth

Industrial communication
IO-Link
Monitoring and maintenance
Real-time maintenance Condition monitoring Predictive maintenance Machine performance Product quality
Application report

Semiconductors: ingot production perfected

How PVA TePla optimises single-crystal growth through automation

PVA TePla AG is a global leading provider of equipment and measuring technology for demanding industrial applications. Its high-tech systems are particularly sought after in the semiconductor industry.

"As a solution provider, we operate globally and are present wherever our customers are. Driven by strong demand from the semiconductor industry, we are currently especially well represented in the Asian market and in the United States," explains Jan Pfeiffer, Managing Director of the PVA TePla Group. With its TechHub in Wettenberg, PVA TePla has positioned itself as a key driver of innovation in materials research for the semiconductor industry.

Silicon carbide – the key to electromobility

The subsidiary PVA Crystal Growing Systems (PVA CGS) can draw on more than 60 years of experience in crystal growing. A particular focus is placed on the production of silicon carbide (SiC) crystals.

"What sets silicon carbide crystals apart is their ability to handle extreme power densities," explains Lukas Ewert, team leader Electrical Design at PVA CGS. “Compared with conventional silicon, the use of SiC enables, for example, the design of smaller batteries with the same power output. The resulting weight reduction is particularly beneficial for electromobility applications."

Extreme conditions require maximum precision

For the production of SiC crystals, PVA TePla designed the SiCma system, which operates according to the Physical Vapor Transport (PVT) method. "In this process, a silicon carbon powder mixture undergoes sublimation in a graphite crucible at around 2,300 °C and deposits onto a seed crystal to form a boule," explains Ewert. "To achieve a high-quality result, temperature and pressure in the process chamber must be precisely controlled throughout the entire crystal growing process. Even the smallest deviations can jeopardise the entire process and lead to significant quality losses." Because such a growth process can take up to three weeks, process monitoring and control must continuously meet the highest standards.

Intelligent sensors ensure stable process conditions

To ensure the required level of precision, PVA relies on IO-Link-capable sensors from ifm. "For example, we use the SV4200 flow sensor from ifm to monitor and keep the cooling water flows constant. This is important not only for maintaining a stable process temperature, but also for protecting housings, pipes and components from overheating and thus from potential damage", explains Ewert.

In addition, the PV8000 pressure sensor monitors the supply and return pressure as well as the temperature of the cooling medium. "Previously, this monitoring was carried out manually. Now we can also retrieve these values via IO-Link and respond to any fluctuations more quickly and effectively," the team leader adds. The AL1202 IO-Link masters collect all sensor data and forward it for central evaluation. The DV signal lamp, which provides users with a visual indication of the current process status, is also controlled via the IO-Link master.

Over many years, we have had only positive experiences with ifm in terms of robustness and reliability in long-term operation. Likewise, when new questions arise or new automation approaches are considered, we can rely on our direct contact at ifm and receive expert support at short notice.

Lukas Ewert Team leader Electrical Design at PVA CGS

About PVA TePla

PVA TePla is a global group of high-tech companies with decades of experience and a strong focus on future innovations. The company develops state-of-the-art systems for vacuum, high-temperature and plasma processes as well as for quality assurance – always in close cooperation with its customers. PVA TePla's customers are mainly active internationally in the semiconductor industry, but also in other high-tech markets such as hydrogen, mobility, battery technology and energy storage.

Over many years, we have had only positive experiences with ifm in terms of robustness and reliability in long-term operation. Likewise, when new questions arise or new automation approaches are considered, we can rely on our direct contact at ifm and receive expert support at short notice.

Lukas Ewert Team leader Electrical Design at PVA CGS

About PVA TePla

PVA TePla is a global group of high-tech companies with decades of experience and a strong focus on future innovations. The company develops state-of-the-art systems for vacuum, high-temperature and plasma processes as well as for quality assurance – always in close cooperation with its customers. PVA TePla's customers are mainly active internationally in the semiconductor industry, but also in other high-tech markets such as hydrogen, mobility, battery technology and energy storage.

IO-Link: more information, greater system transparency

IO-Link has long been established as a manufacturer-independent standard for digital sensor communication in automation technology. Compared with conventional binary and analogue interfaces, IO-Link enables the transmission of high-resolution process values as well as comprehensive diagnostic information. Users benefit from standardised data structures, reduced cabling effort and seamless integration into control systems and IIoT architectures.

The technology supports the transmission of multiple measured values per device, event-driven diagnostics and remote device parameter setting. This results in improved system transparency, optimised maintenance and measurable savings in set-up and operating costs.

Digitalisation as the key factor for system availability

These aspects also play a central role at PVA TePla. "Digitalisation is extremely important for us, especially with the SiCma system," emphasises Lukas Ewert. "These systems are often installed in large numbers in production halls. Loading and unloading are usually fully automated. Our systems must be able to communicate with higher-level systems so that operators can monitor the process status centrally at any time." PVA TePla uses ifm’s comprehensive IO-Link portfolio as the basis for this.

Predictive maintenance for maximum production efficiency

PVA is also working intensively on predictive maintenance concepts in order to provide early indication of upcoming maintenance requirements or process deviations. "This allows operators to maintain maximum machine availability while consistently achieving the highest possible product quality," explains Ewert. The sensors from ifm supply the data required to continuously monitor system condition and to detect potential issues before they result in costly downtime.

Silicon crystal growth using the Czochralski process

PVA places similarly high demands on silicon crystal growth using the Czochralski process. In these systems, silicon ingots up to 3.50 metres in length are grown by slowly pulling a seed crystal from molten silicon at a temperature of around 1,400 °C. The resulting wafers are used primarily in the semiconductor industry and form the basis for a wide range of electronic components.

Low-vibration processes for the highest product quality

"In the SC32 system, automation technology is implemented as a combination of IO-Link and ProfiNet,! explains Ewert.
"We use IO-Link wherever we want to extract more detailed information from the sensors. For example, we use the SM8000 for monitoring and controlling the cooling circuit." This magnetic-inductive flow sensor measures not only the flow rate but also the temperature of the medium.

In addition, PVA uses the three-axis IO-Link vibration sensor VVB3 to monitor the two process drives. The VVB3 detects vibrations along three measurement axes and calculates indicators for evaluating the machine condition. Information on fatigue, friction, impacts or bearing wear is transmitted conveniently via IO-Link.

"Extremely low vibration levels during the pulling process are essential to ensure ingot quality. The transmitted data also allows us to monitor the condition of the gear units and the drive shaft very precisely and to schedule maintenance activities at an early stage."

Reliable components for long-term operation

PVA TePla’s systems are designed for continuous operation over many years. "For this reason, all components, sensors in particular, must deliver consistently precise performance over the long term", emphasises Lukas Ewert.

"Over many years, we have had only positive experiences with ifm in terms of robustness and reliability in long-term operation. Likewise, when new questions arise or new automation approaches are considered, we can rely on our direct contact at ifm and receive expert support at short notice."

Diffusion bonding for the most demanding material requirements

ifm solutions are also used in diffusion bonding technology, another business area of PVA TePla. This solid-state joining process is used, for example, to produce cooling plates for the semiconductor industry, which must meet the highest requirements in terms of strength and corrosion resistance. Patrick Müller, Team Leader Diffusion Bonding at PVA Löt- und Werkstofftechnik GmbH, explains: "To achieve the desired results, process conditions such as temperature, pressure, vacuum and the applied force must be closely monitored throughout the process, which can last several weeks in some cases. The flow sensors from ifm we use to monitor the cooling circuit ensure that the system does not overheat at any point during the process, but remains in a safe operating state."

User-friendliness as added value

Another advantage of ifm’s solutions is their ease of use. Müller highlights the clear, intuitive design of the sensors: "As an operator, you can see at a glance what condition the machine is in. Another clear benefit is how easily older machines can be retrofitted with the sensors. It is effectively plug and play." This user-friendly design not only simplifies day-to-day operation, but also reduces training requirements for operating personnel.

A collaborative partnership as the foundation for innovation

At PVA TePla, the long-standing cooperation with ifm as an automation partner is highly valued: "I’d describe our collaboration with ifm as very cooperative, reliable and based on trust," summarises Lukas Ewert. "We can always approach our contacts directly and work together to drive innovation and automation projects forward."

Conclusion

The requirements in high-tech materials manufacturing are extremely demanding, particularly in terms of precision, reliability and availability. With ifm as its automation partner, PVA TePla successfully meets the challenges associated with advanced crystal growing processes.

Download application report (PDF)
What is your success with ifm?

Have you implemented an interesting application with hardware or software from ifm? How do our sensors help to optimise your process operations? Let us know! We will be happy to present your solution and share your know-how with a large audience – free of charge, of course.