• Products
  • Industries
  • IIoT & Solutions
  • Service
  • Company

Precise level detection amid dust and rock

Efficiency
Costs
Case Study

Radar sensors that provide reliable data even in environments with limestone dust

Higher system
availability

Reliable level
monitoring

Low
maintenance

Results

  • Higher system availability
  • Precise and reliable level monitoring
  • Low-maintenance solution compared to photoelectric systems

The challenge

Lime is an indispensable natural substance used, for example, in the production of steel, as a fertiliser or even in the extraction of sugar. Before lime can be spread on the field, it must be quarried and processed. First, the lumps of rock weighing several tonnes are broken down using crushers. The material is then sieved according to grain size.

A central process step is monitoring the level in the gyratory crusher. A defined limit value must not be exceeded in order to avoid overfilling, especially as the crusher is continuously fed via a conveyor belt. The harsh, dusty ambient conditions make reliable measurement difficult. Nevertheless, precise level monitoring is essential for smooth and safe operation.

Our customer

Fels-Werke GmbH

Fels-Werke GmbH is a leading supplier of lime, limestone and mineral mixtures in Europe. The company extracts around 4 million tonnes of limestone every year at 11 different locations in Germany and the Czech Republic.

Our customer

Fels-Werke GmbH

Fels-Werke GmbH is a leading supplier of lime, limestone and mineral mixtures in Europe. The company extracts around 4 million tonnes of limestone every year at 11 different locations in Germany and the Czech Republic.

The solution – why ifm?

The R1D100 radar sensor from ifm provides reliable level monitoring in this demanding, dusty environment. Thanks to its large angle of aperture, it precisely detects the crushing chamber and thus plays a key role in preventing overfilling.

 

Case Study: Precise and reliable level monitoring

These topics might also be interesting for you: