- Level sensors overview
- Technology overview
Technology overview - level sensors
Impedance spectroscopy
Deposits and foam often make reliable level detection difficult. The impedance spectroscopy technology measures the electric and magnetic field strength at multiple frequencies between 50…200 MHz range. Each medium creates a unique signature profile across this high frequency spectrum sweep. At each point, three measurements are made:
- Attenuation (dampening) of the electromagnetic field
- Conductance of the electric field (ability to conduct an electric current)
- Permittivity (ability to polarize particles) of the magnetic field
When the medium is present, these measurements match the profile. With no medium present or only residue present, the measurements do not match. When the measured profile falls in the green switching zone, the output of the sensor changes state.
Other media have different profiles. Using IO-Link, the medium process values can be evaluated and used to distinguish one material from another, i.e., oil vs. water, whole milk vs. 2% milk, etc.
Features:
- Suppression of residue build-up and foam.
- Flush sealing PEEK sensor tip meets 3A requirements.
- 316L stainless steel body for robustness.
All versions are programmable, but factory default settings are available for water-based media, oil-based / powder media, and high sugar-content media.
Guided wave radar (gwr)
The gwr operating principle uses electromagnetic pulses in the nanosecond (microwave) range. The sensor head transmits the pulses and the pulses travel down the metal probe (guide). When the wave hits the medium, it is reflected back, collected by the metal probe, and guided to the sensor head. The time difference between the transmitting and receiving pulse (time-of-flight) is directly proportional to the distance measurement.
For proper decoupling of the radar pulse, a metal launching plate at least 6” square or 6” diameter is required. If the tank has a metal lid, that can act as the launching plate.
For oil-based media, the fluid surface does not reflect the radar pulse. Rather, it is dispersed into the media. To intensify and contain the signal, we must use a coaxial tube accessory.
When using the coaxial tube, the launching plate as described above is not necessary. This makes mounting easier. However, bridging between the probe and coaxial tube due to solids, emulsions, etc. can cause false level indication. The coaxial tube can be used with water-based media as well and the tube can be cut to length to match the probe.
Features:
- 3A authorized Clean-Out-of-Place (COP) design for some models
- Pressure rating up to 580 psi for some models
- 316L materials of construction
- Immune to dust, fog and steam
Hydrostatic pressure
Hydrostatic pressure is the force per area exerted by a column of liquid and it is a function of the height of the container, not the container’s overall shape or volume. The equation for hydrostatic pressure is:
If the density and specific gravity of the fluid is known, the height (or level) of the fluid can be determined from the hydrostatic pressure measurement. The common unit of measure in North America is inches of water column or inH2O. ifm has many sensors with displays that read in inH2O, but since this is unit of measure of pressure, any other unit of measure of pressure can be used and converted in the PLC. This means that using hydrostatic pressure for level measurement is virtually limitless for the maximum range.
A common hydrostatic pressure application is measuring the level of liquid in a closed tank. A blanket of inert gas may be used to prevent the liquid from oxidizing, such as CO2 on top of a tank of beer. In this case, differential pressure can be calculated using two pressure sensors. The one at the top measures the gas pressure and the one at the bottom measures the gas pressure plus the pressure due to the liquid. The pressure of the liquid only (and therefor the level of the liquid) is the difference in the two measurements.
Capacitive point level (Kxxxxx article numbers)
Capacitive sensors detect any material with or without contact. With ifm’s capacitive proximity sensors, the user can adjust the sensor’s sensitivity to detect liquid or solids even through non-metal tanks.
For successful level detection using capacitive sensors, make sure:
- The vessel wall is non-metal
- The vessel wall is less than ¼” – ½” thick
- There is no metal in the immediate vicinity of the sensor
- The sensing face is placed directly on the vessel wall
- Both the sensor and the vessel are grounded at the same potential
Capacitive continuous level (Lxxxxx article numbers)
ifm’s LK and LT continuous level sensors consist of 16 individual capacitive sensors that are stacked and multiplexed.
Each cell evaluates its surroundings to determine if it is covered by the media. The microprocessor evaluates all 16 cells to determine the media level.
The LK and LT families have built-in overflow protection. The algorithm that monitors overflow is independent from the general level measurement. This way, if the outputs fail to switch as desired and the level continues to rise, the overflow protection forces the outputs to switch.
Additionally, the LT series provides a separate output for medium temperature.
Ultrasonic
Ultrasonic sensors rely on the detection of sound waves reflecting off the surface to measure level. The medium surface reflects sound waves and the distance is determined via time-of-flight measurement.
Unlike photoelectric sensors, the medium’s color, transparency and reflectivity do not affect ultrasonic technology.
Ultrasonic sensors exhibit a high degree of immunity to moisture and dust. The sensing face vibrates at a very high frequency and sheds excess moisture and dust before these substances can negatively affect the performance. However, temperature extremes may affect the accuracy since the speed of sound varies with temperature.
Photoelectric
The O1D laser distance sensor uses pmd time-of-flight technology to measure the distance to the medium surface. The time-of-flight principle monitors the time it takes for a photon of light to travel to the surface and back. The signal is then processed by a receiver element.
This technology is not appropriate for measuring the level of clear liquids. It can be used only for opaque liquids and solids.