You probably do not come from: Namibia. If necessary, change to: United States
  1. moneo: IIoT platform
  2. Products
  3. moneo configure
  4. moneo configure PLC Tools

moneo configure PLC Tools add-on

Simple GSDML parameter setting of IO-Link devices

GSDML files describe the ProfiNet device IO-Link master gateway and function like a "driver" for ProfiNet devices. They contain all relevant parameters and are necessary to configure the device in the Siemens TIA (Totally Integrated Automation) portal / S7-Classic.

However, the integration and, thus, also the display of the IO-Link device parameters is not standard and often requires additional programming effort.

With the new toolbox - moneo configure PLC Tools - ifm now offers you a simple GSDML parameter setting tool as the first feature of this toolbox.

The GSDML files of the ifm masters of the AL14xx series and of the AL1304-07 type can be configured and integrated into the control environment in 3 steps. Add the device parameters that are important to you to the GSDML file yourself, export them and implement them in the TIA Portal. This eliminates the need to read data sheets and set the correct bits, and you need very little time to adapt the GSDMLs to your requirements.

Simple GSDML parameter setting of ifm IO-Link master gateways (AL14xx and AL1304-07) with moneo configure PLC Tools.

User-friendly: Using your predefined files, a tool for all IO-Link devices and automated transfer of the settings when devices are replaced will reduce the time and effort required.

Clear: Enjoy the clearly arranged interface of moneo configure and access the parameters of the IO-Link device directly in the TIA portal as well.

moneo licences

Get advice from our experts

Together we will make your project successful.

Convinced? Just get in touch. We will accompany you on your way. To meet your requirements, our ifm system sales team will support you right from the start - ranging from strategic consulting to the development of individual software and hardware solutions and the corresponding implementation and further services.