Monitoring the reservoir level in hydraulic power units

Hydraulic power unit

Monitoring the reservoir level in hydraulic power units

Application description


Oil level and oil temperature in hydraulic power units
An ifm level sensor of the LK10 series continuously detects the level in the hydraulic power unit. The level can be controlled within the set limits using the operating switching output. In addition, critical process states such as overflow of the vessel can be directly monitored using the overflow switch point.

The LED display on the unit directly shows the current level.

Products for this application