• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • my ifm
  1. TSM clamp-on RTD
  2. Setup and support
  3. Device configuration

TP temperature plug configuration for use with the TSM clamp-on RTD

You can configure the TP plug via the IO-Link interface. For additional help, check our installation instructions or FAQs, or contact our Application Engineers at 800-441-8246.

Calibration of the TP temperature plug

The new TP temperature plug offers users various setting options. Customers can adjust the COF (zero-point offset) and the CGA (calibration gain/slope) of the attached RTD element to align with their calibration.

CGA calibration factor: The CGA (Calibration Gain Adjustment) is a setting that adjusts the slope, or gradient, of the temperature measurement curve to better fit specific applications. You can fine-tune how the sensor interprets temperature changes by adjusting the CGA percentage. This process allows for more precise alignment with your process requirements.  The default setting is 100%, but it can be adjusted between 50% and 200% for customization.

Figure 1:
MW: Measured value
V0: Measurement characteristic at factory setting
V1: Measurement characteristic after offset by +50%
V2: Measurement characteristic after offset by -50%c

cOF Zero Point Correction: The cOF (Correction Offset Factor) allows you to fine-tune the sensor's zero-point to correct for any slight inaccuracies in measurement due to ambient conditions. If the sensor shows a consistent difference between its readings and the actual process temperature, adjusting the cOF can bring the sensor into alignment by shifting its baseline. You can set the cOF within a range of ±10°C, in small steps for precision.

Figure 2:
1: Output signal
2: Process value
V0: Curve of measured values at factory setting
V1: Curve of measured values after offset by +1°C
V2: Curve of measured values after offset by -1°C

Adjustment examples

Example 1: Deviation is linear
Calibration point 0ºC 100ºC
TP calibration results -1ºC 99ºC
COF +1
CGA Unchanged at 100%
TP adjustment results 0ºC 100ºC

 

Example 2: Deviation is not linear
Calibration point 0ºC 100ºC
TP calibration results -1ºC 101ºC
COF +1
CGA v98%
TP adjustment results 0ºC 100ºC

See FAQ: Offset error for 2 or 3 - wire Pt100/Pt1000 connected to a TP:

Configuration with moneo

moneo | configure is a user-friendly software package that enables easy programming and visualization of all ifm IO-Link enabled sensors (V1.0 and V1.1) as well as other manufacturers' IO-Link enabled sensors (V1.1).  The software can be downloaded here: moneo | configure.

Smart phone running the moneo blue app and the EIO330 bluetooth adapter

 

moneo | blue is an app that runs on your Apple or Android smart phones and provides access to all parameters, process values and diagnostics from all sensors connected to an IO-Link master. The Bluetooth™ adapter, EIO330, connects to one port of the IO-Link master and the app can be downloaded free of charge from the Apple App Store or from Google play.