- SDP gap distance sensor
- Setup and support
- Device configuration
SDP Gap distance sensor: Device configuration
The following will guide you through key programming steps for the SDP air gap sensors. More details can be found below on this page.
Common programming features
All of ifm's process sensors, including the SDP air gap sensor, use similar terminology for programming. We highlight the features used most often here. Refer to the Operating Instructions manual found under the "Downloads" tab at the product datasheet page for more details on these and other features.
Switching outputs
- Hno -- hysteresis normally open: Output turns on when the distance set point (SP) is reached and stays on until the distance drops below the reset point (rP)
- Hnc -- hysteresis normally closed: Output turns off when the distance set point (SP) is reached and stays off until the distance drops below the reset point (rP)
- Fno -- window normally open: Output turns on when the distance is between the high limit (FH) and low limit (FL)
- Fnc -- window normally closed: Output turns off when the distance is between the high limit (FH) and low limit (FL)
Analog outputs
- ASP -- analog start point: The measured distance where the analog signal equals 4 mA
- AEP -- analog end point: The measured distance where the analog signal equals 20 mA
- MAW -- initial value of the non-scaled measuring range
- MEW -- final value of the non-scaled measuring range
The chart shows how the analog signal and display information changes when the flow rate is above / below the scaled or non-scaled measuring ranges. This feature is useful in for your process control and troubleshooting issues.
The minimum scaled measuring range is available on the product datasheet.
Display and indications
The SDP gap distance sensors display measured distance, flow rate, and pressure at a glance. Other display indications:
- LED for switching status of output 1
- LED for switching status of output 2
- Display showing current process values or menu / parameters for setup
- Up / down arrows for selecting parameters and changing parameter values
- Enter button to enter the programming menu and confirm the parameter setting value
General use of pushbuttons
| 1 | Press Enter (E) once to enter programming mode. |
|---|---|
| 2 | Press Up or Down arrow (U/D) to view parameters or additional menus. |
| 3 | To change setting, press Enter (E) and then Up or Down arrow (U/D) and hold until the progress bar competes. Then press Up or Down arrow (U/D) to toggle through options. |
| 4 | When desired value is reached, press Enter (E) to confirm the setting. |
Set the gap distance switchpoint
Most gap measurement applications are go / no go. In these cases, the switchpoint can be set using the pushbuttons.
| 1 | Press E to enter programming mode. |
|---|---|
| 2 | Press D until "EF" extended functions is displayed. Press E to confirm. |
| 3 | Press D until "OUT1" is displayed. Press E to configure the output. |
| 4 | "SEL1" is displayed. Press E to change the desired process value (distance, flow, or pressure) is displayed. Press E to confirm. |
| 5 | Press D until "ou1" is displayed. Press E to change the output to desired switching configuration. Press E to confirm the setting. |
| 6 | Press D and "SP1" or "FH1" is displayed. Press E to confirm. |
| 7 | Press U/D to enter the value representing the set point or high limit. Press E to confirm setting. |
| 8 | Press D until "rP2" or "FL1" is displayed. Press E to confirm. |
| 9 | Press U/D to enter the value representing the reset point or low limit. Press E to confirm setting. |
| 10 | Press D until the unit is returned to the "Run" mode. |
Scale the analog signal
Output 2 is available for an analog signal for gap distance, flow rate, or pressure. The value to be scaled must be selected first.
| 1 | Press E to enter programming mode. |
|---|---|
| 2 | Press D until "EF" extended functions is displayed. Press E to confirm. |
| 3 | Press D until "OUT2" is displayed. Press E to configure the output. |
| 4 | "SEL2" is displayed. Press E to change the desired process value (distance, flow, or pressure) is displayed. Press E to confirm. |
| 5 | Press D until "ou2" is displayed. Press E to change the output to "I" for analog signal. Press E to confirm the setting. |
| 6 | Press D and "ASP2" analog start point for output 2 is displayed. Press E to confirm. |
| 7 | Press U/D to enter the value representing the analog start point (4 mA). Press E to confirm setting. |
| 8 | Press D until "AEP2" analog end point for output 2 is displayed. Press E to confirm. |
| 9 | Press U/D to enter the value representing the analog end point (20 mA). Press E to confirm setting. |
| 10 | Press D until the unit is returned to the "Run" mode. |
Enter the number and diameter of nozzles
Accurate distance measurement requires the sensor to know how many nozzles and the size of the nozzles the application uses.
| 1 | Press E to enter programming mode. |
|---|---|
| 2 | Press D until "EF" extended functions is displayed. Press E to confirm. |
| 3 | Press D until "CFG" is displayed. Press E to enter the basic configuration menu. |
| 4 | Press D until "NOZ" is displayed. Press E to enter the number of nozzles. Press E to confirm the setting. Note: Only 1...5 nozzles can be entered. For more than 5 nozzles, enter "None" and refer to the operating instructions for details. |
| 5 | Press D and "diA" is displayed for nozzle diameter. Enter the inner diameter and press E to confirm. |
| 6 | Press D until the unit is returned to the "Run" mode. |
Configuration with software
moneo|configure SA is a user-friendly software package that enables easy programming and visualization of all ifm IO-Link enabled sensors (V1.0 and V1.1) as well as other manufacturers' IO-Link enabled sensors (V1.1). The software can be downloaded here: moneo | configure.
- Parameter data record management -- Easy setup and replacement of IO-Link devices
- One tool for all IO-Link devices -- Manufacturer-independent device setup with integrated IODD management
- Dynamic cockpit view -- Visualize real-time process values and parameters of connected devices