The principle of operation is based on a capacitive measuring cell.
- Voltage is applied between two electrodes and a moisture-absorbing dielectric material is positioned between the electrodes.
- Air from the environment is constantly exchanged with the dielectric material until an equilibrium is established and the capacitance between the electrodes is measured.
- As humidity in the environmental air changes, the capacitance also changes.