• Products
  • Markets
  • IIoT & Solutions
  • Company
  • Resources
  • my ifm

Logic layer functions: Verifying code orientation [Video]

More image-based code reading videos

Area Description Watch video
  Overview Features and setup​
Explore all of the main features of the image-based code reader and see how simple it is to program the device.​
     
  General setup One-button teach function​
In this video, we demonstrate how to setup the device using the one-button teach functionality.​
1D and 2D codes in a single application
In this video, we demonstrate how to setup the device to read 1D and 2D codes in a single application using the free vision assistant software.
Adjusting lighting conditions​
In this video, we demonstrate how to adjust for varying lighting conditions. 
Working with Regions of Interest (ROI)​
In this video, we demonstrate how to setup code reading using regions of interest.
     
  IO-Link integration How to setup IO-Link connection
In this video, we demonstrate how to setup an IO-Link connection in the vision assistant software. ​
How to setup QR code reading​
In this video, we demonstrate how to setup QR code reading using the IO-Link connection in the vision assistant software. 
How to change the running application
In this video, we demonstrate how to change the running application using the IO-Link connection in the vision assistant software. 
How to map the 28 IO-Link bytes to a PLC
In this video, we demonstrate how to send more than 28 bytes of data from the device to a PLC using the IO-Link connection. 
     
  Logic layer functions Logic layer: verifying code content​
In this video, we demonstrate how to create the logic layer in the vision assistant software to verify code content.​
Logic layer: verifying code orientation​
In this video, we demonstrate how to create the logic layer in the vision assistant software to verify code orientation.
Logic layer: verifying code presence​
In this video, we demonstrate how to create the logic layer in the vision assistant software to verify code presence.
Logic layer: verifying code quality​
In this video, we demonstrate how to create the logic layer in the vision assistant software to verify code quality.​
Logic layer: replicating and replacing devices​
In this video, we demonstrate how to replicate settings and replace devices with automatic parameterization.
Logic layer: verifying code placement​
In this video, we demonstrate how to create the logic layer in the vision assistant software to verify code placement.​