Monitor the condition of the rotor brake via remote diagnostics in order to plan maintenance in a targeted manner.
Reliably monitor the cooling of the generator and the lubrication of the generator bearings.
Determine the exact holding position to exclude tripping hazards.
Use the quality of the oil to draw conclusions about the condition of the powertrain.
Operate the wind turbine in such a way that dangerous resonance is avoided.
The rotor lock is monitored to ensure that the rotor is locked against turning during maintenance work.