You probably do not come from: Namibia. If necessary, change to: United States

Connection of the smart valve sensor to the fieldbus

 

Most field devices can be connected to a fieldbus.

This also applies to the smart valve sensor. The device data is transmitted to the masters via IO-Link. Different master versions allow connection to EtherCAT, EtherNet/IP, Modbus TCP, PROFIBUS, PROFINET IO or TCP/IP.

Example of an article list for the connection to PROFINET IO