You probably do not come from: Namibia. If necessary, change to: United States

Grégoire – Autonomous line guidance for grape harvesters

Mobile machines
Agricultural and forestry machines
Monitoring and maintenance
Application report

Automatic grape harvesting with ifm

Autonomous line guidance without GPS for mobile agricultural machines

With EasyPilot, the manufacturer of multi-equipment carriers and harvesters, Grégoire , has created a sensor-assisted automatic line guidance system that boasts a precision of 3 cm without needing a GPS position signal.

No other beverage holds so many secrets and divides so many opinions as wine. Wine: The Italians claim it as their national beverage, and the cup of the everlasting covenant of the Christian faith is filled with it – for in wine is truth: “in vino veritas”.

One truth about wine is that it is necessary to harvest grapes to produce it. And in our days, which are marked by technological progress, the most important question is: man or machine?

The romanticised image of the grape harvest, which we often see in movies and which will surely have inspired one or the other Hollywood star to buy their own vineyard, actually looks quite different in reality. Considering that in Germany alone the average citizen drinks about 20 litres of wine per year, it becomes quite obvious how much work has to be done in a short space of time by about 80,000 German winemakers who cultivate and harvest wine on an area of about 102,000 hectares.

Given these figures, how is it possible to be successful?

Success through technology: Many winemakers use state-of-the-art harvesting machines like grape harvesters instead of manual labourers. Grape harvesters offer various advantages. One hectare, for example, can be harvested in 3 to 5 hours. Achieving the same result with manual labour requires 40 to 60 workers.

How does an automatic grape harvester function?

The French company Grégoire is a manufacturer of grape harvesters. Their grape harvesters can additionally be equipped with an automatic line guidance system: the “EasyPilot”. This system boasts a precision of 3 cm without depending on satellite signals. The grape row is detected by a 3D camera sensor (type O3M) from ifm which measures the distance to the nearest surface for each pixel using time-of-flight technology, thus detecting the general properties of the vines. Inaccuracies caused by vine branches from the side or high grass can be excluded.

While the grape harvester moves over the vines, it creates a tunnel beneath the driver’s cab. In this tunnel, shaking rods made of food-grade plastic fix and shake the trellises. These vibrations shake the vines, so that the grapes fall off. They tumble on a conveyor belt that transports them to stainless steel containers. Suckers remove unwanted elements such as leaves and twigs.

Another 3D sensor is mounted on top of the grape harvester’s driver cab. This sensor is aimed at the ground and determines the height and thickness of the trellis. Once the sensor signal has been processed, a virtual guiding track is generated that visualises the grape row as a model. This model is used as a basis to calculate the ideal route for the harvester to take.

When the machine is in the grape row, the driver starts the EasyPilot via the screen in the cab. Once the system has been started, all the driver needs to do is have an eye on the operating speed and the tools – everything else is taken care of automatically by the system. At the end of the grape row, a visual and acoustic signal informs the driver that the harvester needs to be turned around to move along the next grape row.

There were times when the time for the grape harvest was ordained by the government. Today, winemakers can decide for themselves, and with the grape harvesters from Grégoire, grapes can be harvested at any time – even at night. It remains to be said that innovation pays off: Grégoire have won the innovation award for their new automatic line guidance system EasyPilot, which is based on the O3M sensor from ifm.

Numerous advantages

Besides the absence of a GPS connection, Grégoire’s system offers many other advantages: precise line guidance even in lots with uneven ground, increased quality of the grape harvest (improved ingress resistance, reduced loss, preservation of the vines), increased steadiness of processes beyond the grape harvest (crop spraying, pruning...), protection of the mechanics, convenience and productivity, application possibilities at day and night, operating speeds of up to 12 km/h. EasyPilot is available as an option for the current GM7, GL7, GL8, GX8 and GX9 models. Most predecessor models equipped with a direction sensor can be retrofitted with the system.

Use of inclination sensors

The inclination sensors installed on the harvester play an indispensable role in ensuring that the machine is constantly aligned vertically, no matter how steep the slope. Only the perfect levelling of the grape harvester, regardless of the terrain, makes it possible to achieve maximum throughput and ensure the safety of the user. Besides, the machine can drive faster, saving valuable working time. The 1-axis inclination sensors (type EC2045) used have a CANopen interface which ensures easy integration into the machine controller.

About Grégoire

Grégoire produces automatically guided or trailed grape harvesters and vineyard sprayers featuring inclination sensors.

About Grégoire

Grégoire produces automatically guided or trailed grape harvesters and vineyard sprayers featuring inclination sensors.

Grape harvester driving along the grape row

Grape harvester with the EasyPilot automatic line guidance system.

Conclusion

Grégoire shows that traditional viticulture and modern harvesting machines complement each other perfectly. The EasyPilot, with its 3D camera, guarantees optimum, smooth line guidance. This ensures that no grape is lost during wine production.

Download the application report now
What is your success with ifm?

Have you implemented an interesting application with hardware or software from ifm? How do our sensors help to optimise your process operations? Let us know! We will be happy to share the know-how with a large audience – free of charge, of course.

Systems for mobile machines

You never know what the next job will entail. But you can make sure that your mobile machines are ideally equipped for every challenge: with the robust and reliable system solutions from ifm. From sensors and cables to displays and controllers, ifm offers a complete range of high-quality components for use in mobile machines, all from a single source. So no matter what the challenge is, you can trust that each part of the system will run smoothly. Learn about all the benefits ifm products have to offer!

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.