You probably do not come from: Namibia. If necessary, change to: United States

Control for automatic mooring systems

Port automation
Efficiency
Costs
Safety
Safety of persons
Case Study

All-in-one solution for ship mooring saves time and costs

Increased and safe handling

More efficient handling speed

Less fuel consumption

Results

  • Fast and safe mooring of vessels
  • Increased handling speed
  • Environmentally friendly thanks to deceased fuel consumption
  • Complete system for automation

The challenge

The demands on logistics in the maritime sec­tor are high. Freight traffic is growing strong­ly worldwide, and cargo handling in the ports must therefore become increasingly productive and efficient. This is the only way to handle the high volume reliably and in due time. At the same time, other requirements have to be met, such as better profitability or more environmen­tally friendly technologies. The mooring of ships is one of the starting points. Manual and thus labour-intensive mooring of ships to the quay wall is often still standard practice here. In case of ferries, propulsion is often used to keep the vessel in position.

For some years now, automated or semi-au­tomated mooring systems have played a very important role in efficient handling of ships and goods. These systems replace manual mooring and therefore save personnel and, thus, costs. To automate its mooring systems, Onearc was looking for a provider that could offer a com­plete solution.

Our customer

ONEARC

Founded in 2017, the Swedish company Onearc had initially focused on consulting services for the port and marine industry. In the following years, Onearc additionally specialised in the development of equip­ment for ports and ships, such as auto­matic mooring systems.

In the meantime, the company has become a market leader in special equip­ment for ship and goods handling in ports and on ships. Consultancy services from the concept phase to commissioning and subsequent maintenance also still repre­sent an important part of the business.

Our customer

ONEARC

Founded in 2017, the Swedish company Onearc had initially focused on consulting services for the port and marine industry. In the following years, Onearc additionally specialised in the development of equip­ment for ports and ships, such as auto­matic mooring systems.

In the meantime, the company has become a market leader in special equip­ment for ship and goods handling in ports and on ships. Consultancy services from the concept phase to commissioning and subsequent maintenance also still repre­sent an important part of the business.

The solution – why ifm?

Onearc‘s mooring systems replace the classic mooring ropes and bollards, making the han­dling of ships in ports more efficient, safer and faster. Of particular importance is the reliabil­ity of these systems. They operate with three hydraulical arms that can hold the ship in posi­tion. Depending on the customer‘s require­ments, these arms are each supplied by a separate power unit. To guarantee reliable and safe operation of the mooring system, pressure and temperature sensors monitor every filter, pressure line and hydraulic unit.

Sensors from ifm are used for this, such as TA3105-type tem­perature transmitters and PT5501-type pressure transmitters, both of which are suitable for use in mobile machines. Via special I/O modules for mobile machines, the sensors are connected to a CR1074 controller that controls the system and at   the same time provides the user interface. A signal lamp can visualise the current status of the system.

With the components from ifm, Onearc was able to implement an automation system in which everything is perfectly coordinated. After the first mooring systems that are automated in this way were put into operation in conjunction with an integrator in Sweden, the system will now go into series production.

Case Study: Control for automatic mooring systems

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.