You probably do not come from: Namibia. If necessary, change to: United States

Sustainability thanks to high availability

Other industries
Industry 4.0
Digitalisation
Monitoring and maintenance
Condition monitoring
Case Study

Condition-based maintenance in the production of pencils

Reliable plant operation

Simple evaluation of
the machine status

Cost savings with
condition-based
maintenance

Results

  • Permanent monitoring of important components in the machine
  • moneo edgeConnect translates sensor data into easy-to-read information
  • Plant downtimes are reliably avoided
  • Condition-based maintenance increases the availability and reduces maintenance costs

The challenge

In the mass production of penls, machine faults can quickly lead to high costs. This not only applies to unplanned machine standstills but also to any scrap that may occur. The material scrap of wood should be reduced to a minimum, espe­cially when aiming for a production that ensures maximum sustainability.

The typical machine downtime due to trouble­shooting, cleaning and machine restart is over two hours and should be avoided for efficien­cy and cost reasons. Permanent monitoring of the production machines for faults is here recommended as a remedy. In the past, only a few LEDs had been installed to indicate faults. Hence, extensive monitoring and diagnosis of the machine’s condition had not been possible.

Our customer

A leading manufacturer of stationery

More than two billion pencils per year for the global market. This incredible amount is produced by a German manufacturer of stationery. The company, which operates several manufacturing sites worldwide, employs a staff of over 8,000.

Their vertical integration is very high: plastic parts for stationery are manufac­tured in-house, for example. And even the
forests where the wood for the pencil production is grown are managed by the company themselves. This way, an impor­tant contribution towards sustainability can be made. Only FSC or PEFC certified wood is used in production.

Our customer

A leading manufacturer of stationery

More than two billion pencils per year for the global market. This incredible amount is produced by a German manufacturer of stationery. The company, which operates several manufacturing sites worldwide, employs a staff of over 8,000.

Their vertical integration is very high: plastic parts for stationery are manufac­tured in-house, for example. And even the
forests where the wood for the pencil production is grown are managed by the company themselves. This way, an impor­tant contribution towards sustainability can be made. Only FSC or PEFC certified wood is used in production.

The solution – why ifm?

In order to implement condition monitor­ing, essential components in the production machines, such as compressors, fans and extrud­ers, have been equipped with vibration and tem­perature sensors. The values recorded in this way provide an insight into the machine’s condition at any time.

An edgeConnect evaluation unit from ifm is used to connect the sensors and transmit the meas­ured values to the moneo RTM software. This module of ifm’s digitisation platform enables the evaluation, monitoring and visualisation of the recorded data.

With the machine condition trend being record­ed, the software can detect imminent faults at an early stage. The diagnostic data provide exact information about the machine status at any time, so that possible faults can often be detected in time and thus avoided. This allows condition-based maintenance to be implement­ed, leading to an increased overall availability of a machine.

Should a fault nevertheless occur during oper­ation, moneo RTM can immediately notify the responsible specialists by e-mail, who can then quickly take care of the troubleshooting. These machine monitoring functions with moneo RTM increase the plant availability while also reducing the costs. The planning reliability achieved with the detection of diagnostic data have convinced customers instantly of the solution.

Sustainability thanks to high availability

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.