• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company

Kollmorgen – 3D camera system for pallet detection

Intralogistics & Mobile Robotics
Warehouse automation and distribution Mobile robots
Application report

Summary

A joint solution from Kollmorgen and ifm demonstrates how pallets can be handled more flexibly in intralogistics. 3D cameras capture the position and orientation of pallets, whilst dynamic load docking enables AGVs to pick them up precisely, even when they are placed in varying positions. This lays the foundation for the reliable deployment of autonomous vehicles in variable intralogistics scenarios.

More flexibility in pallet handling

How Kollmorgen and ifm are making AGVs and AMRs smarter

Kollmorgen is an international company specialising in drive technology and automation solutions.

The innovation and development centre for mobile robotics and vehicles in logistics is located in Mölndal, near Gothenburg. There, Kollmorgen is developing a comprehensive automation platform for leading manufacturers of automated guided vehicles (AGVs) and autonomous mobile robots (AMRs). This ranges from vehicle software and hardware to tools for set-up and fleet management systems that enable safe and efficient operation in intralogistics.

New functions are continuously tested and optimised under real-life conditions at the company’s own test centre which provides the ideal environment for working with sensor specialist ifm to develop a camera-based solution for dynamic load handling and bring it to series production.

The challenge: precision in mixed human–robot environments

Many warehouses today rely on AGVs, AMRs and manual processes in parallel. Where people place pallets and vehicles later pick them up, precision determines efficiency. In classic rigid systems, pallets must be placed precisely within a defined field; deviations lead to downtime or manual reworking. “Yet vehicles depend on precision – and the human factor is not always reliable enough,” explains Johan Loebbert, Application Engineer, Kollmorgen AMS, describing the initial situation in rigid systems.

Typical problem areas range from unloading a truck in the receiving area to transferring pallets to buffer zones: the ideal parking spot is often occupied, markings are worn, angles and depths vary. This results in delays in the flow of materials. At the same time, there is increasing pressure to operate heterogeneous fleets in a scalable manner without compromising process reliability. Kollmorgen was looking for a solution that would bridge the gap between human flexibility and vehicleside precision, prevent failures and, at the same time, be easy to integrate into existing vehicle architectures.

The solution: dynamic load docking with ifm camera and PDS app

The answer lies in the combination of Kollmorgen’s Dynamic Load Docking and an ifm camera system with PDS (Pallet Detection System) functionality. Dynamic load docking refers to a process that is primarily used in automated guided vehicles (AGVs) to pick up or set down loads precisely and efficiently, even while the vehicle or load is still moving slightly.

At its heart is an app that recognises the position, orientation and dimensions of a pallet in the camera’s field of view. “In this case, we use ifm’s 3D camera system with PDS function in conjunction with our solution for dynamic load docking,” explains Johan Loebbert. “In the receiving area, a person can place the pallet in a general area in a variable position and at any angle. The AGV then takes a 3D image, determines the exact position and generates an individual travel trajectory to safely pick up the pallet.”

The technical added value is already evident in the integration: install the camera, connect it to the vehicle CPU and controller, perform a quick calibration process and some fine tuning – done, virtually plug and play. The development was a joint project between Kollmorgen and ifm: “The collaboration with ifm was outstanding. ifm developed the PDS solution while we tested our dynamic load docking. Thanks to continuous feedback, we were able to further optimise the functionality,” concludes Johan Loebbert. Even after the market launch, the teams remain in contact to ensure quality and support globally.

Camera platform from ifm

The versatile O3R perception platform forms the technological basis for reliable pallet detection on autonomous guided vehicles (AGVs). The central processing of image and sensor data in the integrated Video Processing Unit (VPU) allows up to six 2D/3D camera heads to be operated synchronously, enabling complete 360° environment detection.

This hardware runs the specially developed “Pallet Detection System” (PDS) software which recognises all standard pallet types regardless of their position and with high precision. The combination of a powerful processing unit, the latest time-offlight imager with high extraneous light stability and a high frame rate ensures robust and dynamic object detection – even under challenging lighting and movement conditions. Thanks to its standardised Docker architecture and support for common development environments such as Python, C++, CUDA and ROS, the system can be flexibly integrated into existing AGV controllers. The O3R platform enables efficient and safe pallet detection, supporting the autonomous approach, positioning and picking up of pallets with precision and reliability – a decisive contribution to the automation and increased efficiency of modern intralogistics processes.

The benefits: greater flexibility, less downtime, higher availability

Camera-based load handling shifts the focus away from rigid rules towards robust processes adapted to the respective situation. The greatest leverage is flexibility: pallets no longer need to be placed in fixed areas. This reduces rework and shortens cycle times in mixed zones where people and vehicles work together. For operators this means: fewer blockages, fewer manual interventions, higher throughputs – with consistent safety. In addition to its process benefits, the solution also impresses in practice with its simple and quick installation. This simplicity facilitates roll-outs across fleets and locations.

Another advantage arises from the openness of the Kollmorgen platform: “Our collaboration with ifm demonstrates just how adaptable and scalable our solution is – in principle, anything can be integrated into the platform,” explains Per Hansson, Partner Channel Coordinator at Kollmorgen AMS. For users, this results in technological sovereignty: the fleet remains expandable, and new functions can be added gradually. “The most important points are efficiency and reliability. There must be confidence that the system will work over time. This is precisely the quality we deliver. We can pool our experience and turn it into a product. It is great to see the problems this solves for our customers,” says Per Hansson. Sensor intelligence and fleet expertise thus combine to create a practical complete package with tangible added value in everyday intralogistics

The collaboration with ifm was outstanding. ifm developed the PDS solution while we tested our dynamic load docking. Thanks to continuous feedback, we were able to further optimise the functionality.

Johan Loebbert Application Engineer, Kollmorgen AMS

About Kollmorgen AMS

Kollmorgen AMS, based in Mölndal (Sweden), develops automation and navigation solutions for automated guided vehicles and mobile robots. The company is part of the Kollmorgen Group and provides software and hardware platforms for industrial logistics and manufacturing worldwide.

The collaboration with ifm was outstanding. ifm developed the PDS solution while we tested our dynamic load docking. Thanks to continuous feedback, we were able to further optimise the functionality.

Johan Loebbert Application Engineer, Kollmorgen AMS

About Kollmorgen AMS

Kollmorgen AMS, based in Mölndal (Sweden), develops automation and navigation solutions for automated guided vehicles and mobile robots. The company is part of the Kollmorgen Group and provides software and hardware platforms for industrial logistics and manufacturing worldwide.

More information of Kollmorgen

Is This the End of Manual Pallet Adjustments in Logistics? Kollmorgen and ifm join forces to bring precision to pallet handling.

 

25 Sep 2025 | 2 minute read

Conclusion

The joint solution from Kollmorgen and ifm combines the best of both worlds: robust, industrial-grade camera sensor technology with a sophisticated automation platform for AGVs and AMRs. If you want to make your intralogistics more resilient, efficient and future-proof, you will find a pragmatic approach here: pallets can be placed flexibly, cameras capture the situation, vehicles operate intelligently – keeping the flow of materials moving.

Download application report (PDF)
What is your success with ifm?

Have you implemented an interesting application with hardware or software from ifm? How do our sensors help to optimise your process operations? Let us know! We will be happy to present your solution and share your know-how with a large audience – free of charge, of course.

These topics might also be interesting for you: