• Products
  • Industries
  • IIoT & Solutions
  • Supply Chain Software
  • Service
  • Company
  1. New products
  2. Sensors
  3. New generation of OGD distance sensors

New generation of OGD distance sensors

Even more performance

The new generation of tried-and-tested distance sensors from the OGD series combines all the advantages of their various predecessor variants in just one device. The user is now presented with a choice of operating modes for optimisation in terms of high measuring distances, maximum precision or high measuring frequencies. This reduces the number of variants while enabling an optimum adaptation to a wide range of applications.

Laser class 2 = range x 2

In laser class 2 version, the OGD doubles its range and detects objects up to 4 metres away. Even dark, reflective or otherwise challenging objects are reliably detected thanks to the new high excess gain (HEG) feature.

Versatile use

The sensors of the OGD series measure distance values with millimetre precision. They are ideal assistants for positioning objects or checking presence, for example in quality control. The reflectance values can also be used, for example for identification in sorting tasks. The areas of application are wide-ranging: whether handling technology, robotics, assembly automation, conveyor technology or logistics; the new OGDs are universal problem solvers for your automation!

Light- or heavy-duty?

The choice is yours. We now offer the OGD in both plastic and stainless steel housings.

User-friendly

As the new OGDs are backward compatible, they can seamlessly adopt the parameter sets of the previous generation when replacing earlier devices.