You probably do not come from: United Arab Emirates. If necessary, change to: United States

Monk Conveyors – IO-Link sensor implementation for optimising conveyor belt equipment

IO-Link sensor implementation for optimising conveyor belt equipment

Thanks to IO-Link, Monk conveyors are able to minimise cabling in the field when building and installing conveyor equipment and machinery. Monk conveyors act as a system integrator: they bring together conveyors and the machines of the costumers as well as the control system into a finished turnkey solution.

There is a lot of field wiring that needs to be done, so the conveyors can work efficiently. ifm's automation solutions are a specific advantage for the conveyor systems because thanks to the IO-Link technology, the cabling itself as well as the wiring time can be reduced, and more visibility and monitoring of the system is possible.

Head start with IO-Link

Head start with IO-Link

Today the user gets completely new options with IO-Link sensors from ifm. The transfer of cyclic and acyclic data, for example, as well as messages in both directions are implemented. And IO-Link has a lot more to offer: noise immunity, no measured value losses, easy sensor replacement, tamper free, identification and wire break detection

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.