You probably do not come from: United Arab Emirates. If necessary, change to: United States

ifm protects your critical assets

Wood industry
Monitoring and maintenance
Condition monitoring
Case Study

Prevent production downtimes with vibration monitoring

67,000 € production losses prevented

27h man hours saved

100% ROI after 9 month

Results

3 bearing faults have been detected within 9 months, which corresponds to a production loss of 67,000 € (including the costs for new motors).

  • Cost of new motor = 1,395 €
  • Time to replace / repair the motor = 3 hours
  • Cost of lost production = 20,930 €
  • Man Hours saved = 9 hours (3 men needed)

Compared to the cost of the vibration training course and the cost of hardware per asset, it was a very worthwhile investment, according to James Jones.

  • Monitoring Hardware per asset = Total cost 1,539 € (1 x VSE100, 4 x VSA001 and cables)
  • Vibration Monitoring Training = Total cost 2,395 €

The challenge

Due to the high demand in their products, keeping production running is a major priority for James Jones. Motors that drive large cutting blades that cut logs into different sizes are critical assets for them. If one of the motors fails, the entire production line comes to a standstill and there is a risk of high production losses. Vibration modules and sensors can help to detect faults before they become serious and to ensure pro­duction uptime.

Vibration monitoring solutions can be very com­plex, sometimes due to the amount of data you cannot understand what you are seeing. With­out a clear focus, it‘s hard to get real results.

Our customer

JAMES JONES & SONS LIMITED

Through five generations of family owner­ship, James Jones & Sons has manufac­tured the widest range of sawn timber products including carcassing, fencing, palletwood, heavy sections and, more recently, engineered timber products and is now regarded as one of the most inno­vative and efficient timber processors in Europe.

The failure of critical assets can lead to high production losses. ifm makes vib­ration monitoring easy! Even beginners can be vibration experts. Production los­ses of  67,000 € were prevented within 9 months.

Our customer

JAMES JONES & SONS LIMITED

Through five generations of family owner­ship, James Jones & Sons has manufac­tured the widest range of sawn timber products including carcassing, fencing, palletwood, heavy sections and, more recently, engineered timber products and is now regarded as one of the most inno­vative and efficient timber processors in Europe.

The failure of critical assets can lead to high production losses. ifm makes vib­ration monitoring easy! Even beginners can be vibration experts. Production los­ses of  67,000 € were prevented within 9 months.

The solution – Why ifm?

Can vibration discussions be simple? Yes they can!

ifm offers vibration training courses for all lev­els which, in combination with the user-friendly hardware, help to achieve real results as quickly as possible. James Jones saw these results after training.

Once the VSE was fitted and had monitored the critical bearing over a couple of weeks, the data showed that the bearing frequency trends were increasing over time on the unit. Based on this information, James Jones decided to remove the unit from service and install a new motor.

However as can be seen in the trend, the bearing frequency levels quickly started to increase again. So more in-depth analysis was required. Know­ing the bearing frequencies enabled an accurate diagnosis of the fault, which showed as an outer race defect.

Due to the large increase in the bearing levels over three days, it was decided to replace the drive end bearing. On inspection of the bear­ing, the outer race damage is visible, the cause is electrical fluting. Now insulated bearings will be fitted solving the Root Cause of the failures.

Case Study: ifm protects your critical assets

Vibration monitoring product overview

The ifm group of companies: our own development and production with high quality standard.

The detection and integrated evaluation of vibration signals serves as a basis for the seamless integration of online condition monitoring into manufacturer-independent automation and control systems.

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.