The integrated, automatic object recognition detects up to 20 stationary or moving objects in the path of a construction vehicle. By comparing the current speed, the motion vector and fixed parameters such as the braking distance, the collision probability is calculated by the 3D sensor and transferred to the machine control system via CAN bus or Ethernet and then signalled to the driver.