Service hotline (020) 8213 2222

Application example Memory Plug

Data storage and parameter setting using the memory plug
The memory plug enables easy copying and saving of sensor parameters. As soon as a data set is stored on the memory plug it can be copied from the plug's memory to a new sensor when a sensor of the same type is connected. This saves time and avoids errors when new parameters are set.

Advantages of the Memory Plug

The memory plug ensures...
  • parameter setting of the IO-Link sensors from all manufacturers if data storage of the devices is effected according to the IO-Link specification V1.1.
  • data storage of parameters for IO-Link devices.
  • parameter storage of connected devices.
  • fast replacement of sensors without new parameter setting in the event of a defect.
  • fast commissioning and sensor programming in series at the desk and during production.
  • configuration verification of the connected sensor.
  • loading of a parameter set from the sensor or the storage via FDT.
  • easy restoration of the factory settings of the memory plug and selection between the two read and write modes.
Click here for more information about the memory plug.
ifm Memory Plug Applikation

IO-Link Memory Plug