New selectors facilitate search for AS-i units
 
 

 

Bookmark and Share
There now is a convenient search function for the creation of an AS-interface system on the internet.

Similar to the selectors for the selection of sensors, there now are product selectors for AS-i masters/controllers, power supplies, input/output modules and AirBoxes. In this interactive product search a selection can be made based on the most important criteria. The matching products will then be displayed in a list which can be refined by means of further criteria. A data sheet is opened by clicking on the article number. With another click the article can be placed in the shopping basket and ordered online.

Here you can find the suitable AS-i masters, controller e units or the suitable gateway.
Control cabinet modules - at a glance for the first time.
Field modules - all available units.
All 24 V and AS-i power supplies in one selector.
AirBox - quickly and easily find the AirBox.